STMicroelectronics, WURTH Elektronik and Element14 have created a Special Project which comprises an STMicroelectronics Motor Control Evaluation kit.
EVLSPIN32G4-ACT Motor control Evaluation Board
STLINK-V3SET Programmer/debugg...
STMicroelectronics, WURTH Elektronik and Element14 have created a Special Project which comprises an STMicroelectronics Motor Control Evaluation kit.
EVLSPIN32G4-ACT Motor control Evaluation Board
STLINK-V3SET Programmer/debug...
Intro
Previously I investigated how to use the GIGA Display's microphone, but now it is time to explore the audio out put, This blog demonstrates how the Arduino GIGA R1 can read a WAV audio file from a USB memory device and play it using its DAC out...
STMicroelectronics and Wurth Elektronik in collaboration with Element14 has put together a development kit to evaluate including the addition of products needed to fully review the development/evaluation products.
Wurth Elektronik and STMicro ar...
After a somewhat bumpy beginning, I am starting the roadtest. The first Arduino Giga R1 board that I received was missing the 24 pin display passthrough connector J5 on the right side below.
The good news is that cstanton was ab...
Intro
The Arduino GIGA R1 kit I am road testing has a display with built in microphone. To test the microphone I am starting with using it to create a VU meter (volume unit meter). All the hardware necessary for this VU meter is included in this plug...
Intro
The Arduino Giga R1 has a camera connector, so of course I want check it out, so I purchased the highest resolution color camera I could find that had the correct connector. This is the Arducam B0462 which uses a 2 megapixel GC2145 camera senso...
Intro
This is the second installment of material that will contribute to a road test of the Arduino GIGA R1 and its LCD.
The Arduino web site has an example of how to display an image stored on a USB memory stick, but it needs the IDE serial monitor...
This is the first installment towards an Arduino GIGA R1 Road Test.
Intro
The Giga R1 WiFi could be the most capable microcontroller so far, both from a computing capability point of view as well as an I/O point of view. On the computing side it has...
B&K Precision DAS60 High Speed Multi-Function Recorder
The B&K Precision DAS60 is the top model in the High-Speed Multi-Function Recorder category and positioned for applications in research, development, maintenance, and power monitoring....
Hello Element14 Community!
This is a short blog post, part of my MultiComp PRO 3D Printer Filament RoadTest, in which I will show how I usually calibrate new filaments for my 3D Printer.
The 3D printer filaments I got for thi...
Introduction
I was very exited and grateful to Element14 to get an opportunity to evaluate Arduino Pro Nicla Voice board. I wanted to use it as an input device for my local chat bot, so it can be always on, and be my digital companion....
Dear Community members,
I m working on Arduino due board Rev 3 version. I have observed that this board gets reset in Random fashion . I unable to find out the reason. If Somebody who has worked more extensively than me on this board,might help...
Table of Contents
True RMS Performances of MP730655
Conclusions
True RMS Performances of MP730655
What means RMS? RMS = root mean square. I am not going to discuss the details of the math formula for RMS here. The basic idea of RMS is to calcula...
Table of Contents
Out-of-Box Review
Some Features and True RMS Performances of MP730655
Out-of-Box Review
I recently received part of the prize from Element14 as the fifth prize winner in NI LabVIEW and Test Automation Beginner’s Course. Th...
In this last part of the Polarfire Video SOC review we'll develop a custom AI network from scratch to use the VectorBlox SDK and run on it on the Polarfire video board. Then we'll try to port a current state of the art like (SOTA) stereo networ...
Introduction
In the previous blog we have seen the data coming from serial device. In this blog, we will see how to monitor the inference result through BLE communication.
Receiving Methods
Android mobile with Nordic Semiconductor’s “NRF...
Introduction
Thanks to E14, I received a RASynBoard dev kit as a part of Road-test. For a small product, this kit has so many features that cannot be covered in a single blog. So, I have decided to split the content into two blogs, each focusing on d...
Intro
I am road testing a Digilent Analog Discovery 3 which included a BNC Adapter accessory module. The adapter connects to the Analog Discovery module via a 30 pin header, but there are no other mechanical fasteners to stabilize the connection. BNC...
VectorBlox SDK Setup
in this part we'll install the VectorBlox SDK and test the example networks on board. The VectorBlox AI accelerator makes use of an SDK that leverages the openVino framework to convert AI networks from floating point format desig...
This part of the Polarfire SOC Video Kit review will detail the installation of the required software for working with the Polarfire Video SOC development board. Ubuntu 22.04 LTS was used for all the development work however similar steps can b...
This is the third and last blog post before the final review for the Rohm BD9G500EFJ-EVK-001 RoadTest. Here, I'm going to explore one of the many tools Rohm has available on its website to assist with the design process.
To get access, you have t...
This is the second part of the Eval Kit BD9G500EFJ-EVK-001 RoadTest. If you have missed the first blog, you can check it out here.
In this blog I'm going to design a buck converter to provide power to one servo. Input power is supposed to be 4s L...
I recently had the good privilege of being selected to receive the Keysight E36731A Battery Emulator and Profiler as part of Element14's roadtest program. Now, batteries might not be everyone’s cup of tea, but having spent some years worki...
First of all, I want to thank element14 and Rohm for this great opportunity: testing the BD9G500EFJ-EVK-001 evaluation board and becoming for the first time a roadtester.
What's special about the BD9G500EFJ-EVK-001 ?
The BD9G500EFJ-EVK-001 is a...