MXO4 Logic Analyser
The MXO4 offers a logic analyser option. All the hardware is built in, but you need to pay for the Mixed Signal upgrade to get the probes and the software key to unlock it. That’ll add £2622 to the base price, so...
Hi all. Hope everyone is safe.
First of all, thank you Element14 and rscasny for choosing me as a finalist for the Road Test. Hope not to disappoint.
I'm going to divide this into several posts to be able to tackle everything and ...
Introduction
In common with an increasing number of oscilloscopes the MXO4 series offers the option of a built-in signal generator and software to allow it to operate as a Frequency Response Analyser.
In the case of the MXO4 the FRA and signal genera...
Recently, I was selected for the review of Nordic's Thingy:53 development platform. I received the parcel last week and it is really cool device.
Here in this small first impression blog I will post some pictures and explain what the dev. kit contain...
The Rohde & Schwarz MXO 4 series oscilloscope arrived about a week ago for a RoadTest review, and I was keen to start using it, but first a little "unboxing" needed to be done.
Michael michaelkellett has a blog wi...
This blog is about my first day with the ‘scope. Because it’s such a complicated instrument, with a lot of features and a definite learning curve, I’m avoiding expressing too much opinion about features or lack of them because I don...
If you missed the subtlety of the Crocodile Dundee reference... these connectors are fantastic. Thank you e14 for the opportunity to try them out.
What are they? Specifically, the MulticompPRO MP series magnetic connectors. ...
This is video HDMI output at 1920x1080 (full HD) @ 60 fps from RASPBERRY PI2 programmed just like any good & high speed ARM based microcontroller without any OS. This means there is no OS inside board.This demonstration also shows all 4 cores of ...
This demonstration shows serial to ethernet conversion. EK-TM4C1294XL KIT (Tiva C launchpad kit) is connected with PC using USB cable. This connections enables onboard debugger & creates Virtual com port on configuring the windows drivers on PC. ...
Here EK-TM4C1294XL KIT (Tiva C launchpad kit) is connected with PC using standard LAN cable. This board is USB powered, so USB cable is connected with PC on other side. We have to pre-configured ip address of PC in same range as ip address configured...
STM8SVLDiscovery kit contains STM8S003K3 MCU connected with X-NUCLEO-IHM07M1 with L6230PD motor driver IC. Motor make: Maxon,Switzerland. Motor: PMSM, low wattage & high torque is connected with motor driver IC. This demonstration shows both cloc...
In the previous blog post I performed several experiments to assess some performance parameters of the MTi-680 from Xsens. In this blog post I will continue with some more experiments with the MTi-680 to see how well it performs. I wil...
HI,
i m Neeraj Gupta. I work in a prominent Defense OEM for developing defense equipment.
I have 16 to 17 year of experience in solving problems/equipment development using embedded systems. I have created solutions fo...
When dealing with high(er) performance pieces of equipment, it's very important to understand what all those numbers in the datasheet mean in the real-world. For example, for a particular use case, you may ask yourself whether you need to use a MTi-6...
Can you share any statics on selected candidates completing reviews for RoadTests they have been awarded?
I just discovered only one of three reviews was completed for the WAGO Terminal Block RoadTest. I was considering making an application for the ...
I'm hoping someone would share their technique for finding all the reviews related to a particular Roadtest?
I have had this struggle for a while but figured at some point I would discover how to navigate to all the posted content for a RoadTest.
My ...
LattePanda 3 Delta – RoadTest
Terms and Conditions
These are the terms and conditions which govern the LattePanda 3 Delta RoadTest contest. This Contest requires participants to submit an application indicating their previous experience wi...
With this part of my roadtest of the PolarFire FPGA I implement an example accelerator design for sorting on it, and I compare it with results from a Xilinx board (Avnet's Ultra96). I always considered such a comparison very interesting and useful, a...
Weller is interested in providing the element14 community a couple of its new soldering platform for a roadtest. It's called the WXsmart.
Here are the documents I was given on this product:
Quick GuidePower UnitWXAir
Here's what it looks li...
In this blog post I will look at how easy (or not) it is to get started with the MTi-680-DK development kit. Although the Roadtest page for MTi-680-DK has several relevant resources linked to it, I will initially assume that page does not exist and s...
Introduction
After carrying out the roadtest of the AVR-IoT Cellular Mini Development Board,, I tried to create a simple project that used this versatile board from Microchip.
The project I want to carry out is that of a simple telemetry sent to a r...