FPGA
  • Technologies
  • More
FPGA
Blog PYNQ and Zynq: the Vitis HLS Accelerator with DMA training - Deep Dive: the data streams between Accelerator IP and ARM processors
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 27 Nov 2021 1:21 PM Date Created
  • Views 3092 views
  • Likes 1 like
  • Comments 0 comments
  • vitis_hls
  • fpga
  • vivado
  • pynq
  • hardware_accelerators
Related
Recommended

PYNQ and Zynq: the Vitis HLS Accelerator with DMA training - Deep Dive: the data streams between Accelerator IP and ARM processors

Jan Cumps
Jan Cumps
27 Nov 2021

This is a supporting post for Part 2: Add the Accelerated IP to a Vivado design.
I'm untangling the different data streams.
There are 3 types of data exchanged between the FPGA and ARM parts of the Zynq:

  • "Business Data": the inputs and outputs to the hardware accelerated logic function. Focus on speed and throughput.
  • "Control Data": the signals used to interact, enable, control, configure the exchange of that business data. 
  • "Other signals": reset, clock. I will not discuss those in this post.

Control Data

The DMA and Accelerated IP blocks use normal speed, AXI Lite, signals to interact with the ARM.
These blocks, signals and busses handle anything that is not related to the fast input/output.
They are supported by a dedicated AXI Interconnect block.
All blocks implement the AXI protocol and know how to work together. For the designer, the only task is to put them on the block design and configure them.

image

In our case, this AXI Interconnect needs two master channels, because it 'll control both DMA IP and Accelerator IP.

Business Data

The input and output data streams have to be as efficient as possible. They use the High Performance AXI channels of the ARM/ZYNQ. And DMA.
The AXI DMA block will be the in-between for bi-directional traffix between ARM DRAM and Accelerator IP.
I can show the flows in two ways. DMA-IP and DMA-ARM, or Input and Output. Im going for the lather.
When you look at each of the flows below, you'll see that there's a linear flow both times.

From DRAM to Accelerated IP

This is the input flow to the accelerated function. Data flows from DRAM to the IP block.

image

The AXI DMA block is the orchestrator, It will use a AXI Interconnect to retrieve a memory block from DRAM, and stream it to the Accelerator IP.
This becomes the input data for the logic implemented inside that IP.
What happens is: data will stream from the ARM's high performance channel S_AXI_HP2 to the IP, with the two AXI blocks managing that flow.

From Accelerated IP to DRAM

This is the other way round. The data that's been transformed inside the Accelerator IP (output data) is streamed to the ARM's DRAM.

image

The AXI DMA again manages the fast flow. Data streams from the IP to the ARM's high performance channel S_AXI_HP0.

 

Pynq - Zync - Vivado series
Add Pynq-Z2 board to Vivado
Learning Xilinx Zynq: port a Spartan 6 PWM example to Pynq
Learning Xilinx Zynq: use AXI with a VHDL example in Pynq
VHDL PWM generator with dead time: the design
Learning Xilinx Zynq: use AXI and MMIO with a VHDL example in Pynq
Learning Xilinx Zynq: port Rotary Decoder from Spartan 6 to Vivado and PYNQ
Learning Xilinx Zynq: FPGA based PWM generator with scroll wheel control
Learning Xilinx Zynq: use RAM design for Altera Cyclone on Vivado and PYNQ
Learning Xilinx Zynq: a Quadrature Oscillator - 2 implementations
Learning Xilinx Zynq: a Quadrature Oscillator - variable frequency
Learning Xilinx Zynq: Hardware Accelerated Software
Automate Repeatable Steps in Vivado
Learning Xilinx Zynq: Try to make my own Accelerated OpenCV Function - 1: Vitis HLS
Learning Xilinx Zynq: Try to make my own Accelerated OpenCV Function - 2: Vivado Block Design
Learning Xilinx Zynq: Logic Gates in Vivado
Learning Xilinx Zynq: Interrupt ARM from FPGA fabric
Learning Xilinx Zynq: reuse and combine components to build a multiplexer
PYNQ version 2.7 (Austin) is released
PYNQ and Zynq: the Vitis HLS Accelerator with DMA training - Part 1: Turn C++ code into an FPGA IP
PYNQ and Zynq: the Vitis HLS Accelerator with DMA training - Part 2: Add the Accelerated IP to a Vivado design
PYNQ and Zynq: the Vitis HLS Accelerator with DMA training - Part 3: Use the Hardware Accelerated Code in Software
PYNQ and Zynq: the Vitis HLS Accelerator with DMA training - Deep Dive: the data streams between Accelerator IP and ARM processors
Use the ZYNQ XADC with DMA part 1: bare metal
Use the ZYNQ XADC with DMA part 2: get and show samples in PYNQ
VHDL: Convert a Fixed Module into a Generic Module for Reuse