Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog 1958 Turntable from the Black Forest - 5: Turntable speed sample testbed with Arduino UNO
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 25 Mar 2015 8:43 PM Date Created
  • Views 2366 views
  • Likes 3 likes
  • Comments 7 comments
  • motor_driver
  • ir_sensor
  • enchanted_player
  • enchanted_objects
  • sample
  • pwm
  • arduino_uno
  • arduino
Related
Recommended

1958 Turntable from the Black Forest - 5: Turntable speed sample testbed with Arduino UNO

Jan Cumps
Jan Cumps
25 Mar 2015

image

 

I'm creating a test setup for the speed sample firmware.
In this post I'm reviewing the speed sensing approach and how the Arduino knows how fast the turntable is spinning.

 

image

 

Where should I measure the speed?

 

There are a number of options. The table has 5 parts where the speed can be measured.

 

image

  • motor: should run at a constant speed all the time, regardless of the selected turntable speed
  • belt: constant
  • stepped pulley: constant
  • idler: dependent on selected speed, moves up and down depending on speed too
  • turntable platter: dependent on selected speed.

 

As it turns out, the easiest candidate is the stepped pulley. Its speed should be constant regardless of the selected platter speed, and it is easy to attach a sensor under it.

For a more detailed explanation of how the record player works, speed calculations and selection of the speed sensor, have a look at these posts:

Vintage Turntable repair: Can I fix a Perpetuum Ebner from 1958 - part 2 - Calculating the Motor Speed

Vintage Turntable repair: Can I fix a Perpetuum Ebner from 1958 - part 7 - Make Speed Sensor from Scrap Parts

Vintage Turntable repair: Can I fix a Perpetuum Ebner from 1958 - part 8 - Sample the Motor Speed with Microcontroller

 

The gist of all the above is that I'm going to measure the speed of that stepped pulley with an infrared sender - receiver pair.

A small piece of mirror glued to the underside of the pulley will reflect the IR beam once per rotation.

We'll get a nice digital signal from that sensor with the same frequency as the pulley speed.

 

More on that in a next post.

The only thing we have to remember for now that that pulley is going to spin at a few 10's of RPMs.

 

Simulating the Speed Sensor

 

We know that the sensor is going to give a signal with the frequency of the spinning pulley.

The signal will be high when the mirror is in front of the IR sensor, and low for the rest of the rotation. The width of the small mirror defines the duty cycle of our sensor output.

 

It's easy to simulate that signal with a signal generator with TTL output and variable duty cycle.

If we set that to a signal within the speed range of that pulley (I've selected 12.5 Hz in my test setup here), and play a bit with the duty cycle, we have a signal that is very similar to the sensor output.

We can change the functuon generator frequency to simulate that the turntable is slowing down or going too fast.

We can play with the duty cycle to test that our firmware will sample the frequency correctly in the real world, and find the minimum size of the mirror.

 

image

 

The Speed Sample Firmware

 

I've looked at several frequency measure examples for the Arduino.

I selected the first one that works together with my PWM solution for the motor driver (1958 Turntable from the Black Forest - 4: Motor control with Infineon Motor Shield and Arduino UNO).

It is avdweb Frequency / period counter for the Arduino.

You can use this library in polling mode (do a measurement when you need it) or in interrupt mode. I chose interrupt mode.

 

In interrupt mode, the frequency polling will happen in the interrupt handler when the sensor signal changes.

Whenever we need to know the speed, we can just look up the value that was collected in the interrupt.

There are only a few pins that can be used with interrupts. You can find more info on the attachInterrupt() help page.

 

The library is not hard to use. This is how you initialize it:

 

// includes for sensor
#include <FreqPeriodCounter.h>

// ...

// variables and constant for sendor
const byte iSensorPin = 3;
const byte iSensoCounterInterrupt = 1; // = pin 3
FreqPeriodCounter sensorCounter(iSensorPin, micros);

 

The next step is to set up the interrupt mechanism. We have a handler that's called when the value on pin 3 changes.

We have to register that handler. And that's it. From that moment the frequency measurement is working.

 

void sensoCounterISR() {
  sensorCounter.poll();
}

void sensorSetup() {
  attachInterrupt(iSensoCounterInterrupt, sensoCounterISR, CHANGE);
}

 

We can get at the last measured frequency anytime. I've created this method for that:

 

long  sensorPeriod() {
  return sensorCounter.period;
}

 

I'm using the period because that's not a floating point. Frequency is 1/period, and that's a float.

For my use, I can work with both period and frequency. Both indicate how fast the table is spinning.

So I avoided the requirement to link in the floating point libraries by sticking with period.

 

That's all.

For testing purposes, I'm logging the period in the main loop of my firmware.

When I change the frequency of my function generator, the Arduino serial monitor has to display the correct period.

When I change the duty cycle on my function generator, the Arduino should ignore that and keep showing the correct period.

 

void setup(void) {
  Serial.begin(9600);
  sensorSetup();

  // ...
}

void loop(void) {

    // ...

  long period = sensorPeriod();
    Serial.println(period);
    delay(1000);
}

 

The Results

 

In the photos and captures below, you can see the results.

The figures on the frequency counter, oscilloscope and Arduino serial monitor match within a reasonable margin.

 

Frequency counterOscilloscopeArduino sampled values
imageimageimage

 

Let's have a closer look at that oscilloscope capture:

 

image

This is an odd capture. The two signals don't have the same time base (one is 33 kHz, the second 15.5 Hz - and still both show stable and well-triggered on the scope).

This is called alternate trigger mode. It's used to show to signals that don't relate to each other in the time dimension.

 

I want to show the PWM signal of my motor control on the oscilloscope to validate that my sample firmware does not impact the motor drive firmware.

So any change of my frequency generator should leave the upper part of the scope unchanged.

Vise versa, if I change the PWM of the motor driver, the sample firmware should still measure the sensor signal correctly.

 

The alternate trigger technique is a good method to show this. You can see if altering one signal has impact on the other.

But don't try to relate the signals to each other. You have to see this display as 'split screen'. Upper and lower part have a different timeline and trigger point.

 

More on the subject of alternate triggers in this video:

 

This video is unavailable.
You don't have permission to edit metadata of this video.

 

In the next post, I'm going to build the sensor and do real world tests.

 

 

Table of Contents
Chapter 1: Fix the turntable
1: Perpetuum Ebner Musical 1
2: A Time to Kill and a Time to Heal
3: Preparation for Motor Drive
4: Motor control with Infineon Motor Shield and Arduino UNO
5: Turntable speed sample testbed with Arduino UNO
6: Turntable Speed Sensor design
7: Control Theory - End of Chapter 1
Chapter 2: First Enchantments
8: Digital Light Organ Enchantment
9: Autonomous Servo Lift
10: SMD Time - Solder the IR Speed Sensor PCB
11: Yelp - who can Help me to Compile and Run my First SAMA5D4 C Program
12: Son et Lumiere - End of Chapter 2
Chapter 3: Taming the Board
13: Breakthrough - Run my own C++ Program on the SAMA5D4
14: Digital Light Organ Input Buffer
15: SAMA5D4 Blinky
16: Scope Creep
17: Audio Sampling with 16-bit ADC ADS8343
18: Sending Files to SAMA5D4 over USB
19: Port my Light Organ from Arduino to SAMA5D4
20: Fast Fourier Transform on the SAMA5D4 - End of Chapter 3
Epilogue: Reaching for the Clouds
21: Right-Sizing my Plans
22: My Own C++ Buffered Sampler on the SAMA5D4
Interlude
23: Building In the Motorized Light Organ
24: Up to the Clouds with Yún
25: Publish or Perish
26: Turntable Finished
Stretch & Boni
Bonus 1a: Remote Light Organ with WiFI pt. 1
Bonus 1b: Remote Light Organ with WiFI pt. 2
Grande Finale: Paho MQTT Client on the SAMA5D4
Related blog
Vintage Turntable repair: Can I fix a Perpetuum Ebner from 1958
Review 1: Atmel SMART SAMA5D4 Xplained Ultra Unboxing and First Steps
Review 2: Atmel SMART SAMA5D4 Xplained Ultra - Building the Libraries from Source
Review 3: Digital Continuous Rotation (360°) Servo Part 1
Review 4: Digital Continuous Rotation (360°) Servo Part 2
Review 5: Atmel SMART SAMA5D4 Xplained Ultra - TCP/IP running
Review 6: Atmel SMART SAMA5D4 Xplained Ultra - LINUX Distro with SSH support
poem
Enchanted Objects: Let's work together to tame the ATMEL SMART SAMA5D4 Xplained Ultra kit
17 bis: Off South...
Review 7: Atmel SMART SAMA5D4 Xplained Ultra - C++ ADC Example on Linux
Review 8: Atmel SMART SAMA5D4 Xplained Ultra - Product Review
Review 9a: Atmel SMART SAMA5D4 Xplained Ultra - Set up ADC Buffer with Hardware Trigger Part 1
Review 9b: Atmel SMART SAMA5D4 Xplained Ultra - Set up ADC Buffer with Hardware Trigger Part 2
Review 10: Atmel SMART SAMA5D4 Xplained Ultra - New Content on AT91.com
1958 Turntable from the Black Forest - Summary of the Enchanted Player Story
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 10 years ago in reply to mcb1 +2
    Here's an action photo of the strobo disk. I'm in Belgium, 50 Hz.
  • mcb1
    mcb1 over 10 years ago +1
    Jan Nice writeup and great link for frequency/period count. I presume your feedback loop has some slugging in it to stop it constantly hunting. My old Dual turntable has cast marks around the platter and…
  • DAB
    DAB over 10 years ago +1
    Nice update. I am not sure just how constant the speed must be to get good sound reproduction. I do like your strobe disk print. I like quick and dirty engineering fixes. DAB
Parents
  • Jan Cumps
    Jan Cumps over 10 years ago

    Preview of the table playing a record, with the Arduino doing a so-so job to maintain a constant speed:

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 10 years ago

    Preview of the table playing a record, with the Arduino doing a so-so job to maintain a constant speed:

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview