FPGA
  • Technologies
  • More
FPGA
Blog Learning Xilinx Zynq: a Quadrature Oscillator - 2 implementations
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 4 Aug 2021 8:32 PM Date Created
  • Views 7021 views
  • Likes 13 likes
  • Comments 23 comments
  • zynq
  • xilinx
  • vivado
  • summer of fpgas
  • pynq
Related
Recommended

Learning Xilinx Zynq: a Quadrature Oscillator - 2 implementations

Jan Cumps
Jan Cumps
4 Aug 2021

shabaz made a Software Defined Radio (SDR) Experiment Board. One of the components is a digital quadrature oscillator.

It's a circuit with 4 PWM outputs that are each 90° shifted.

image

In Shabaz' blog, the oscillator is made with flip-flops, and controlled by an external function generator.

Because it's the Summer of FPGAs, I'm proposing 2 FPGA based alternatives.

They work identical, generate the same frequency (input / 4), but the approach is different.

One works by replaying a predefined output pattern on the 4 outputs, with one clock delay for each output.

The second one by calculating the first channel based on a counter value, and left shifting the data through the outputs.

 

The entity is identical for the two approaches:

 

library IEEE;
use IEEE.STD_LOGIC_1164.ALL;
use IEEE.NUMERIC_STD.ALL;

entity quadrature_oscillator is
  Port (
    i_clk: in std_logic;
    i_nReset: in std_logic;
    o_outputs: out std_logic_vector (3 downto 0)
   );
end quadrature_oscillator;

 

This is the first implementation.

The pattern used to define the outputs is 0011001.

Each of the pins continuously cycles through a (different!) range of 4 bits of the pattern, on the cadence of the clock.

pin 0 from 3 to 6: 1100

pin 1 from 2 to 5: 0110

pin 2 from 1 to 4: 0011

pin 3 from 0 to 3: 1001

They do this at the same time, in parallel.

You can see that this generates an output where each of the pins is 90° shifted.

 

architecture Behavioral of quadrature_oscillator is
  signal s_pattern: std_logic_vector (6 downto 0) := "0011001";
  signal s_counter: natural range 0 to 3 := 0;

begin
process (i_clk, i_nReset)
begin
--  if i_nReset = '0' then
--    s_counter <= 0;
--  els
  if rising_edge(i_clk) then
    if s_counter = 3 then
      s_counter <= 0;
    else
      s_counter <= s_counter + 1;
    end if;
    o_outputs(0) <= s_pattern(s_counter + 3);
    o_outputs(1) <= s_pattern(s_counter + 2);
    o_outputs(2) <= s_pattern(s_counter + 1);
    o_outputs(3) <= s_pattern(s_counter);
  end if;
end process;

end Behavioral;

 

The second implementation takes a different approach.

The data is the output vector is shifted 1 position to the left. That generates 90° phase shift.

I only have to take care that I set the LSB correct each time. For that, I use the MSB of the counter, inversed.

The counter is 2 bits. It cycles 00 -> 01 -> 10 -> 11.

If you take the MSB each time, inversed, you get 1100.

That's the identical as the output of pin 0 in the first implementation. The left-shift does the rest of the magic for the other 3 pins.

 

architecture Behavioral of quadrature_oscillator is
  signal s_counter: UNSIGNED (1 downto 0) := "00";
  signal s_buffer: std_logic_vector (3 downto 0) := (others => '0');

begin
process (i_clk, i_nReset)
begin
  if i_nReset = '0' then
    s_counter <= "00";
    s_buffer <= (others => '0');
  elsif rising_edge(i_clk) then
    if s_counter = "11" then 
      s_counter <= (others => '0');
    else
      s_counter <= (s_counter) + 1;
    end if;
    s_buffer <= s_buffer (2 downto 0) & not(s_counter(1));
    o_outputs <= s_buffer;
  end if;
end process;

end Behavioral;

 

I've attached Vivado project and Jupyter notebook. Implementation #2 is active, approach #1 is commented out.

The VHDL for #2 is adapted, see https://www.element14.com/community/groups/fpga-group/blog/2021/08/04/learning-xilinx-zynq-a-quadrature-oscillator#comme… .

Latest source on github: https://gist.github.com/jancumps/0a1b2692ddfd6edc79e8487adc66539e

 

Which design do you prefer? Or do you have an alternative?

 

Pynq - Zync - Vivado series
Add Pynq-Z2 board to Vivado
Learning Xilinx Zynq: port a Spartan 6 PWM example to Pynq
Learning Xilinx Zynq: use AXI with a VHDL example in Pynq
VHDL PWM generator with dead time: the design
Learning Xilinx Zynq: use AXI and MMIO with a VHDL example in Pynq
Learning Xilinx Zynq: port Rotary Decoder from Spartan 6 to Vivado and PYNQ
Learning Xilinx Zynq: FPGA based PWM generator with scroll wheel control
Learning Xilinx Zynq: use RAM design for Altera Cyclone on Vivado and PYNQ
Learning Xilinx Zynq: a Quadrature Oscillator - 2 implementations
Learning Xilinx Zynq: a Quadrature Oscillator - variable frequency
Learning Xilinx Zynq: Hardware Accelerated Software
Automate Repeatable Steps in Vivado
Learning Xilinx Zynq: Try to make my own Accelerated OpenCV Function - 1: Vitis HLS
Learning Xilinx Zynq: Try to make my own Accelerated OpenCV Function - 2: Vivado Block Design
Learning Xilinx Zynq: Logic Gates in Vivado
Learning Xilinx Zynq: Interrupt ARM from FPGA fabric
Learning Xilinx Zynq: reuse and combine components to build a multiplexer
PYNQ version 2.7 (Austin) is released
PYNQ and Zynq: the Vitis HLS Accelerator with DMA training - Part 1: Turn C++ code into an FPGA IP
PYNQ and Zynq: the Vitis HLS Accelerator with DMA training - Part 2: Add the Accelerated IP to a Vivado design
PYNQ and Zynq: the Vitis HLS Accelerator with DMA training - Part 3: Use the Hardware Accelerated Code in Software
PYNQ and Zynq: the Vitis HLS Accelerator with DMA training - Deep Dive: the data streams between Accelerator IP and ARM processors
Use the ZYNQ XADC with DMA part 1: bare metal
Use the ZYNQ XADC with DMA part 2: get and show samples in PYNQ
VHDL: Convert a Fixed Module into a Generic Module for Reuse

 

Attachments:
quad_osc_jupyter.zip
quadrature_oscillator.zip
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 5 years ago in reply to jc2048 +4
    These are the GUI settable parameters: Then there's a bespoke Clocking Wizard IP that can be attached to clock signals in fabric: I've not tested it yet, I just put one on the block design and checked…
  • Jan Cumps
    Jan Cumps over 5 years ago +3
    The Vivado / Zynq / Pynq artifacts: Block diagram: Constraints: Jupyter notebook: I've used one of the Zync fabric clocks as input. Any clock works, and output will be clock/4. Here, the input clock was…
  • fmilburn
    fmilburn over 5 years ago +3
    Impressive that you did this so quickly and with so little code
Parents
  • jc2048
    jc2048 over 5 years ago

    Here is another alternative, running on my VIDOR 4000.

     

    image

     

    But this one is bland and boring, because it's just a very simple finite-state machine. Here's the VHDL:

     

    ---------------------------------------------------------------
    --- Filename: quad.vhd                                      ---
    --- Target device: 16CL016YU256C8G                          ---
    ---                                                         ---
    --- Quadrature generator                                    ---
    --- using classic two-process FSM (finite state machine)    ---
    ---                                                         ---
    --- Jon Clift 5th August 2021                               ---
    ---                                                         ---
    ---------------------------------------------------------------
    --- Rev    Date         Comments                            ---
    --- 1.0    05-Aug-21                                        ---
    ---------------------------------------------------------------
    
    
    library IEEE;
    use IEEE.std_logic_1164.all;  
    ---use IEEE.numeric_std.all;  
    use ieee.std_logic_arith.all;
    use ieee.std_logic_unsigned.all;
    
    entity quad_top is port(
    
       --- system signals
       CLKi:             in std_logic;
       RESn:             in std_logic;
      
       --- MKR PINS
       MKR_D:            out std_logic_vector(3 downto 0);
       
       --- SDRAM
       SDRAM_CK:         out std_logic;
       SDRAM_CSn:        out std_logic;
       SDRAM_CKE:        out std_logic;
      
       --- NINA module
       WM10_RESn:        out std_logic
    
       );
    end quad_top;
    
    architecture arch_quad_top of quad_top is
    
    type StateType is (deg0, deg90, deg180, deg270);
    signal present_state, next_state: StateType;
    signal quad: std_logic_vector(3 downto 0);
    signal next_a, next_b: std_logic;
    
    begin
    
       --- first process runs from the 48MHz clock input on CLKi
       --- this moves us on to the next state
       --- and latches the new outputs
    
        clocked_stuff: process (CLKi) begin
            if (CLKi'event and CLKi = '1') then
                present_state <= next_state;
                quad(0) <= next_a;
                quad(1) <= next_b;
                quad(2) <= not next_a;
                quad(3) <= not next_b;
                end if;
          end process clocked_stuff;
    
       --- second process is all the combinatorial stuff
       --- ...what the next state is
       --- and what the outputs are going to be when clocked
    
        combi_stuff: process (present_state) begin
          case present_state is
             when deg0 =>
                next_state <= deg90;
                next_a <= '1';
                next_b <= '0';
             when deg90 =>
                next_state <= deg180;
                next_a <= '1';
                next_b <= '1';
             when deg180 =>
                next_state <= deg270;
                next_a <= '0';
                next_b <= '1';
             when deg270 =>
                next_state <= deg0;
                next_a <= '0';
                next_b <= '0';
             end case;
          end process combi_stuff;
    
          --- connect servo outs to the MKR pins
    
          MKR_D <= quad;
    
          --- hold some of the unused, board hardware components in inactive state
             
          SDRAM_CK <= CLKI;
          SDRAM_CSn <= '1';
          SDRAM_CKE <= '1';
             
          WM10_RESn <= '0';
    end arch_quad_top;

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jc2048
    jc2048 over 5 years ago

    Here is another alternative, running on my VIDOR 4000.

     

    image

     

    But this one is bland and boring, because it's just a very simple finite-state machine. Here's the VHDL:

     

    ---------------------------------------------------------------
    --- Filename: quad.vhd                                      ---
    --- Target device: 16CL016YU256C8G                          ---
    ---                                                         ---
    --- Quadrature generator                                    ---
    --- using classic two-process FSM (finite state machine)    ---
    ---                                                         ---
    --- Jon Clift 5th August 2021                               ---
    ---                                                         ---
    ---------------------------------------------------------------
    --- Rev    Date         Comments                            ---
    --- 1.0    05-Aug-21                                        ---
    ---------------------------------------------------------------
    
    
    library IEEE;
    use IEEE.std_logic_1164.all;  
    ---use IEEE.numeric_std.all;  
    use ieee.std_logic_arith.all;
    use ieee.std_logic_unsigned.all;
    
    entity quad_top is port(
    
       --- system signals
       CLKi:             in std_logic;
       RESn:             in std_logic;
      
       --- MKR PINS
       MKR_D:            out std_logic_vector(3 downto 0);
       
       --- SDRAM
       SDRAM_CK:         out std_logic;
       SDRAM_CSn:        out std_logic;
       SDRAM_CKE:        out std_logic;
      
       --- NINA module
       WM10_RESn:        out std_logic
    
       );
    end quad_top;
    
    architecture arch_quad_top of quad_top is
    
    type StateType is (deg0, deg90, deg180, deg270);
    signal present_state, next_state: StateType;
    signal quad: std_logic_vector(3 downto 0);
    signal next_a, next_b: std_logic;
    
    begin
    
       --- first process runs from the 48MHz clock input on CLKi
       --- this moves us on to the next state
       --- and latches the new outputs
    
        clocked_stuff: process (CLKi) begin
            if (CLKi'event and CLKi = '1') then
                present_state <= next_state;
                quad(0) <= next_a;
                quad(1) <= next_b;
                quad(2) <= not next_a;
                quad(3) <= not next_b;
                end if;
          end process clocked_stuff;
    
       --- second process is all the combinatorial stuff
       --- ...what the next state is
       --- and what the outputs are going to be when clocked
    
        combi_stuff: process (present_state) begin
          case present_state is
             when deg0 =>
                next_state <= deg90;
                next_a <= '1';
                next_b <= '0';
             when deg90 =>
                next_state <= deg180;
                next_a <= '1';
                next_b <= '1';
             when deg180 =>
                next_state <= deg270;
                next_a <= '0';
                next_b <= '1';
             when deg270 =>
                next_state <= deg0;
                next_a <= '0';
                next_b <= '0';
             end case;
          end process combi_stuff;
    
          --- connect servo outs to the MKR pins
    
          MKR_D <= quad;
    
          --- hold some of the unused, board hardware components in inactive state
             
          SDRAM_CK <= CLKI;
          SDRAM_CSn <= '1';
          SDRAM_CKE <= '1';
             
          WM10_RESn <= '0';
    end arch_quad_top;

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to jc2048

    I've added your implementation to the Vivado project I've attached to the main blog. It works perfectly.

    • Cancel
    • Vote Up +3 Vote Down