• Products and Partners
    Products and Partners
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
FPGA
  • Technologies
  • More
FPGA
Blog Learning Xilinx Zynq: Hardware Accelerated Software
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 8 Aug 2021 6:02 PM Date Created
  • Views 4761 views
  • Likes 6 likes
  • Comments 5 comments
  • vitis_hls
  • summer_of_fpgas
  • zynq
  • jupyter
  • vivado
  • pynq
  • vitis
Related
Recommended

Learning Xilinx Zynq: Hardware Accelerated Software

Jan Cumps
Jan Cumps
8 Aug 2021

The main target for Zynq family FPGAs is: compute systems with hardware acceleration.

It's architecture focuses on being able to stream data efficiently between ARM and FPGA submodules.

The FPGA can then perform manipulations in hardware that take too long in software.

The tool chain supports this. The Vitis HLS IDE's only goal is to convert C functions to FPGA IPs..

 

I have edited this article for Vivado and Vitis HLS version 2020.2.

The examples are updated for these versions, and work with Pynq 2.6 and 2.7.

You get the working sources right now via git clone -b image_v2.7_2020.2 https://github.com/mariodruiz/PYNQ-HelloWorld.git --recursive.

A merge request is open to het it into the Xilinx repo https://github.com/Xilinx/PYNQ-HelloWorld/tree/image_v2.7.

Hardware Accelerated Image Resize Algorithm

 

As proof of concept,  Xilinx adapted OpenCV so that you can build functions and filters in hardware.

I'm reviewing such an example: image resize.

This demo performs the same exercise twice: resize an image from 3840 * 2160 to  1920 * 1080

  • using the ARM processor to execute OpenCV resize calls
  • using the same function, implemented inside the FPGA fabric.

 

The results:

in software, it took 1.03 s. In hardware, 210 ms.

The test is both times done in a loop, taking the fastest execution as benchmark. This to take in account optimising, caching, incidental OS activity, ...

The time taken is from having the original image in memory,  to when the algorithm has finished writing the resized image to memory.

 

Resize executed in ARM processors Resize executed in FPGA fabric
image image

 

 

 

The Accelerated Resize Function Design

 

This is done in Vitis HLS. The example uses the Xilinx OpenCV port and calls its resize() function.

The C code (full):

 

void resize_accel(stream_t& src, stream_t& dst,
                  int src_rows, int src_cols,
                  int dst_rows, int dst_cols) {
    // Convert stream to xf::cv::Mat
    axis2xfMat<DATA_WIDTH, TYPE, HEIGHT, WIDTH, NPIX>(src, src_mat);
    // Run xfOpenCV kernel:
    xf::cv::resize<INTERPOLATION, TYPE, HEIGHT, WIDTH, HEIGHT, WIDTH, NPIX, MAXDOWNSCALE>(src_mat, dst_mat);
    // Convert xf::cv::Mat to stream
    xfMat2axis<DATA_WIDTH, TYPE, HEIGHT, WIDTH, NPIX>(dst_mat, dst);
    
}

 

Vitis HLS converts this into an FPGA IP (both Verilog and VHDL source are generated).

image

 

This IP can then be used in Vivado

 

The Accelerated Resize Function Used

 

You can use this generated IP similar to other IPs in Vivado. In the image below, it's the orange block.

Inputs and outputs are interfaced with the ARM controllers via the AXI interface.

 

 

 image

image

 

Install on Pynq Board

 

This is straightforward.

You open a Linux terminal. There is one available from the Jupyter home page of your board. Or you can use PuTTY, etc.

Then follow the Quick Start. The two notebooks with ARM and FPGA implementations will become available

 

 

 

Building the example from source

If you want to have the Vivado and Vitis HLS projects available in your 2020.2 install, that's possible.

 

Clone the HelloWorld git, with subprojects.

no longer needed to clone Mario D Ruiz' project. It's now merged with the Xilinx repo

git clone -b image_v2.7_2020.2 https://github.com/mariodruiz/PYNQ-HelloWorld.git --recursive

git clone -b image_v2.7_2020.2 https://github.com/Xilinx/PYNQ-HelloWorld.git --recursive

Vitis HLS Project

 

start Vitis 2020.2 TCL
cd <where you cloned>\PYNQ-HelloWorld\boards\ip
vitis_hls -f build.tcl -tclargs ./vitis_lib/vision/L1/include/ resize/resize/impl/ip/component.xml

Vivado Project

start Vivado 2020.2 TCL

cd <where you cloned>/PYNQ-HelloWorld/boards/Pynq-Z2/resizer

It may be needed to edit ressizer.tcl. Comment below if you did not have to do this.
replace set_property ip_repo_paths ../../ip [current_project]

with set_property ip_repo_paths ../ip [current_project]

vivado -mode batch -source resizer.tcl -notrace
vivado -mode batch -source build_bitstream.tcl -notrace

 

 

You now have the sources and projects for the accelerated function and the Vivado FPGA design.

 

 

Pynq - Zync - Vivado series
Add Pynq-Z2 board to Vivado
Learning Xilinx Zynq: port a Spartan 6 PWM example to Pynq
Learning Xilinx Zynq: use AXI with a VHDL example in Pynq
VHDL PWM generator with dead time: the design
Learning Xilinx Zynq: use AXI and MMIO with a VHDL example in Pynq
Learning Xilinx Zynq: port Rotary Decoder from Spartan 6 to Vivado and PYNQ
Learning Xilinx Zynq: FPGA based PWM generator with scroll wheel control
Learning Xilinx Zynq: use RAM design for Altera Cyclone on Vivado and PYNQ
Learning Xilinx Zynq: a Quadrature Oscillator - 2 implementations
Learning Xilinx Zynq: a Quadrature Oscillator - variable frequency
Learning Xilinx Zynq: Hardware Accelerated Software
Automate Repeatable Steps in Vivado
Learning Xilinx Zynq: Try to make my own Accelerated OpenCV Function - 1: Vitis HLS
Learning Xilinx Zynq: Try to make my own Accelerated OpenCV Function - 2: Vivado Block Design
Learning Xilinx Zynq: Logic Gates in Vivado
Learning Xilinx Zynq: Interrupt ARM from FPGA fabric
Learning Xilinx Zynq: reuse and combine components to build a multiplexer
PYNQ version 2.7 (Austin) is released
PYNQ and Zynq: the Vitis HLS Accelerator with DMA training - Part 1: Turn C++ code into an FPGA IP
PYNQ and Zynq: the Vitis HLS Accelerator with DMA training - Part 2: Add the Accelerated IP to a Vivado design
PYNQ and Zynq: the Vitis HLS Accelerator with DMA training - Part 3: Use the Hardware Accelerated Code in Software
PYNQ and Zynq: the Vitis HLS Accelerator with DMA training - Deep Dive: the data streams between Accelerator IP and ARM processors
Use the ZYNQ XADC with DMA part 1: bare metal
Use the ZYNQ XADC with DMA part 2: get and show samples in PYNQ
VHDL: Convert a Fixed Module into a Generic Module for Reuse
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 5 years ago +1
    I'm going to try make an own project with acceleration, now that I understand a bit how the development cycle ticks .
Parents
  • Jan Cumps
    Jan Cumps over 5 years ago

    I'm going to try make an own project with acceleration, now that I understand a bit how the development cycle ticks .

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Andrew J
    Andrew J over 5 years ago in reply to Jan Cumps

    Early days yet: made the ubiquitous 'Hello World', created a boot loader for the device, flashed lEDs and read a button state, but that's all PS.  I'm still working on the basics but will be attempting to recreate what you've been doing in your blogs Jan.  Keep them coming, they are being read!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Andrew J
    Andrew J over 5 years ago in reply to Jan Cumps

    Early days yet: made the ubiquitous 'Hello World', created a boot loader for the device, flashed lEDs and read a button state, but that's all PS.  I'm still working on the basics but will be attempting to recreate what you've been doing in your blogs Jan.  Keep them coming, they are being read!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to Andrew J

    Andrew J  wrote:

     

    Early days yet: made the ubiquitous 'Hello World', created a boot loader for the device, flashed lEDs and read a button state, but that's all PS.  I'm still working on the basics but will be attempting to recreate what you've been doing in your blogs Jan.  Keep them coming, they are being read!!

    My blogs use the Pynq precompiled Linux image, so I'm not boot-loading or bare-metaling.

    I'm following the Xilinx 4-part workshops, to see if I can do the core things that are explained in the next webinar on the Pynq board I have here...

    But until now I've focused on custom FPGA bitstreams on an existing Linux with Pynq.