Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog 1958 Turntable from the Black Forest - 12: Son et Lumiere - End of Chapter 2
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
  • Author Author: Jan Cumps
  • Date Created: 25 Apr 2015 9:44 AM Date Created
  • Views 997 views
  • Likes 4 likes
  • Comments 3 comments
  • enchanted_player
  • enchanted_objects
Related
Recommended

1958 Turntable from the Black Forest - 12: Son et Lumiere - End of Chapter 2

Jan Cumps
Jan Cumps
25 Apr 2015

image

 

 

We're halfway through the story. It's time to close chapter 2.

 

image

 

Sound and Light

 

In chapter 1 I turned a broken vintage turntable into a working one. The defect AC motor was thrown out and replaced by a microcontroller driven one.
This turns the table into an autonomous device that knows how fast it should pin. It adapts its behavior to that knowledge.

That is a tactical change - from defect to working.

But a first enchantment is achieved. The table still looks the same as the day it was built, but under the hood - invisible to the eye - it has a brain ...

 

And in this chapter, the table became visible enchanted.

I added a speed indicator. This 3-LED mini-module listens to the speed regulator and shows what it's doing. Read chapter 3 for the higher power plans with this module and the Infineon RGB shield.

 

image

 

Next was the light organ. This is fully implemented in firmware. It uses Fast Fourier Transform to analyze bass, middle and treble parts of the signal.

It's also an autonomous module

At this moment, the organ drives three LEDs - and that is going to stay like that, but once more: read chapter 3 for the higher power plans with this module and the Infineon RGB shield.

 

image

 

Servo Enchantment

 

I added a mechanical arm to the organ.

 

image

 

The arm has a sole (autonomous image ) responsibility to hide the light organ inside the belly of the table. The light organ asks the motor to pop op when it feels like animating the scene.

That's how the whole enchanting set-up is done. All options can be removed or plugged in as desired. The whim of the day can have an impact on the table.

 

image

 

And as a preparation for the next chapter, I've started to make some more space under the turntable.

I'll have to check if this impacts the strength of the case. First tests are promising.

 

 

 

BeforeAfter
imageimage

 

 

side story: why do you see photos from another turntable in this post?

 

Because I fixed that this month.

 

image

A lady asked my wife if I could fix her 1964 Philips console. It's a tube radio and amplifier with an automatic changer turntable.

The radio worked but the turntable was defect. A good working (but newer,  lower in the food chain) changer from 1970 had to offer its life to fix the console.

That's how it goes in enchanted stories. They are often hard and violent. The life of looser isn't worth much in the fairy-tale world if it's not Walt Disney who writes the script.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image
You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image
You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image
You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image
You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

(in total 20 minutes of video. Still well below Robert Peter Oakes' average image)

 

 

 

Table of Contents
Chapter 1: Fix the turntable
1: Perpetuum Ebner Musical 1
2: A Time to Kill and a Time to Heal
3: Preparation for Motor Drive
4: Motor control with Infineon Motor Shield and Arduino UNO
5: Turntable speed sample testbed with Arduino UNO
6: Turntable Speed Sensor design
7: Control Theory - End of Chapter 1
Chapter 2: First Enchantments
8: Digital Light Organ Enchantment
9: Autonomous Servo Lift
10: SMD Time - Solder the IR Speed Sensor PCB
11: Yelp - who can Help me to Compile and Run my First SAMA5D4 C Program
12: Son et Lumiere - End of Chapter 2
Chapter 3: Taming the Board
13: Breakthrough - Run my own C++ Program on the SAMA5D4
14: Digital Light Organ Input Buffer
15: SAMA5D4 Blinky
16: Scope Creep
17: Audio Sampling with 16-bit ADC ADS8343
18: Sending Files to SAMA5D4 over USB
19: Port my Light Organ from Arduino to SAMA5D4
20: Fast Fourier Transform on the SAMA5D4 - End of Chapter 3
Epilogue: Reaching for the Clouds
21: Right-Sizing my Plans
22: My Own C++ Buffered Sampler on the SAMA5D4
Interlude
23: Building In the Motorized Light Organ
24: Up to the Clouds with Yún
25: Publish or Perish
26: Turntable Finished
Stretch & Boni
Bonus 1a: Remote Light Organ with WiFI pt. 1
Bonus 1b: Remote Light Organ with WiFI pt. 2
Grande Finale: Paho MQTT Client on the SAMA5D4
Related blog
Vintage Turntable repair: Can I fix a Perpetuum Ebner from 1958
Review 1: Atmel SMART SAMA5D4 Xplained Ultra Unboxing and First Steps
Review 2: Atmel SMART SAMA5D4 Xplained Ultra - Building the Libraries from Source
Review 3: Digital Continuous Rotation (360°) Servo Part 1
Review 4: Digital Continuous Rotation (360°) Servo Part 2
Review 5: Atmel SMART SAMA5D4 Xplained Ultra - TCP/IP running
Review 6: Atmel SMART SAMA5D4 Xplained Ultra - LINUX Distro with SSH support
poem
Enchanted Objects: Let's work together to tame the ATMEL SMART SAMA5D4 Xplained Ultra kit
17 bis: Off South...
Review 7: Atmel SMART SAMA5D4 Xplained Ultra - C++ ADC Example on Linux
Review 8: Atmel SMART SAMA5D4 Xplained Ultra - Product Review
Review 9a: Atmel SMART SAMA5D4 Xplained Ultra - Set up ADC Buffer with Hardware Trigger Part 1
Review 9b: Atmel SMART SAMA5D4 Xplained Ultra - Set up ADC Buffer with Hardware Trigger Part 2
Review 10: Atmel SMART SAMA5D4 Xplained Ultra - New Content on AT91.com
1958 Turntable from the Black Forest - Summary of the Enchanted Player Story
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 11 years ago in reply to DAB +2
    In that case, I 'll revert my changes and give it back. I estimate that it would take me 3 to 4 hours to get it back to the non-working turntable it was in when I got it. I haven't damaged a single thing…
  • Workshopshed
    Workshopshed over 11 years ago +1
    Top quality stuff, fitting the mechanical things does take lots of time and at the end of the day most of it will be hidden!
  • DAB
    DAB over 11 years ago +1
    Great post and cool idea. What happens if the guy who gave you the turntable wants it back? DAB
Parents
  • DAB
    DAB over 11 years ago

    Great post and cool idea.

     

    What happens if the guy who gave you the turntable wants it back?image

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 11 years ago

    Great post and cool idea.

     

    What happens if the guy who gave you the turntable wants it back?image

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 11 years ago in reply to DAB

    In that case, I 'll revert my changes and give it back.

    I estimate that it would take me 3 to 4 hours to get it back to the non-working turntable it was in when I got it.

    I haven't damaged a single thing during my exercise here.

     

    It would be a bummer for my enchanted story, but I guess I'd find something else to enchant in that case.

    Great ideas are born when things don't go as expected image.