Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog 1958 Turntable from the Black Forest - Interlude
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
  • Author Author: Jan Cumps
  • Date Created: 27 May 2015 8:07 PM Date Created
  • Views 1986 views
  • Likes 5 likes
  • Comments 11 comments
  • enchanted_player
  • enchanted_objects
Related
Recommended

1958 Turntable from the Black Forest - Interlude

Jan Cumps
Jan Cumps
27 May 2015

image

 

No electronics in today's post. Just a few pictures of the work on the sub-chassis.

I'm avoiding to drill holes in the nice turntable coffer. I'm crafting a light carton base that nicely fits inside the turntable.

The material I use is from my son's school project. He's building an architectural model of a house.

 

image

 

Building the sub-chassis

 

It's just the fancy name for a piece of carton. As prototype I used part of a pizza box.

 

image

 

I made that fit using the trial and error method.

image

 

Then I used it as template for the cardboard.

 

image

 

image

 

This is the end result: a nicely fitting mounting plate.

After cutting it out, I re-traced the sides with an extra line of red sharpie to give it that professional finished look image.

 

image

 

Having this removable base plate will make it easier to work on the different parts.

And I can take everything out at once when I have to revert the turntable to its original state.

 

 

Table of Contents
Chapter 1: Fix the turntable
1: Perpetuum Ebner Musical 1
2: A Time to Kill and a Time to Heal
3: Preparation for Motor Drive
4: Motor control with Infineon Motor Shield and Arduino UNO
5: Turntable speed sample testbed with Arduino UNO
6: Turntable Speed Sensor design
7: Control Theory - End of Chapter 1
Chapter 2: First Enchantments
8: Digital Light Organ Enchantment
9: Autonomous Servo Lift
10: SMD Time - Solder the IR Speed Sensor PCB
11: Yelp - who can Help me to Compile and Run my First SAMA5D4 C Program
12: Son et Lumiere - End of Chapter 2
Chapter 3: Taming the Board
13: Breakthrough - Run my own C++ Program on the SAMA5D4
14: Digital Light Organ Input Buffer
15: SAMA5D4 Blinky
16: Scope Creep
17: Audio Sampling with 16-bit ADC ADS8343
18: Sending Files to SAMA5D4 over USB
19: Port my Light Organ from Arduino to SAMA5D4
20: Fast Fourier Transform on the SAMA5D4 - End of Chapter 3
Epilogue: Reaching for the Clouds
21: Right-Sizing my Plans
22: My Own C++ Buffered Sampler on the SAMA5D4
Interlude
23: Building In the Motorized Light Organ
24: Up to the Clouds with Yún
25: Publish or Perish
26: Turntable Finished
Stretch & Boni
Bonus 1a: Remote Light Organ with WiFI pt. 1
Bonus 1b: Remote Light Organ with WiFI pt. 2
Grande Finale: Paho MQTT Client on the SAMA5D4
Related blog
Vintage Turntable repair: Can I fix a Perpetuum Ebner from 1958
Review 1: Atmel SMART SAMA5D4 Xplained Ultra Unboxing and First Steps
Review 2: Atmel SMART SAMA5D4 Xplained Ultra - Building the Libraries from Source
Review 3: Digital Continuous Rotation (360°) Servo Part 1
Review 4: Digital Continuous Rotation (360°) Servo Part 2
Review 5: Atmel SMART SAMA5D4 Xplained Ultra - TCP/IP running
Review 6: Atmel SMART SAMA5D4 Xplained Ultra - LINUX Distro with SSH support
poem
Enchanted Objects: Let's work together to tame the ATMEL SMART SAMA5D4 Xplained Ultra kit
17 bis: Off South...
Review 7: Atmel SMART SAMA5D4 Xplained Ultra - C++ ADC Example on Linux
Review 8: Atmel SMART SAMA5D4 Xplained Ultra - Product Review
Review 9a: Atmel SMART SAMA5D4 Xplained Ultra - Set up ADC Buffer with Hardware Trigger Part 1
Review 9b: Atmel SMART SAMA5D4 Xplained Ultra - Set up ADC Buffer with Hardware Trigger Part 2
Review 10: Atmel SMART SAMA5D4 Xplained Ultra - New Content on AT91.com
1958 Turntable from the Black Forest - Summary of the Enchanted Player Story
  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 11 years ago +2
    Nice work. You did have me guessing with the first few pictures ...then I realised it was a house ... not a housing. Mark
  • Jan Cumps
    Jan Cumps over 11 years ago in reply to Workshopshed +2
    This works better: I can't remember where I scavenged it from, but it's multi-strand, thin and flexy. www.youtube.com/watch
  • Jan Cumps
    Jan Cumps over 11 years ago +2
    Medieval style adaption of the proto board to the Yún
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    I love this project image

     

      That turntable that you've got to work with is gorgeous, It's amazing to see it transforming into something of use these days!

     

    I'd totally be getting carried away with thinking about new features to be putting on it 

     

     

    Lucie

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 11 years ago

    I love this project image

     

      That turntable that you've got to work with is gorgeous, It's amazing to see it transforming into something of use these days!

     

    I'd totally be getting carried away with thinking about new features to be putting on it 

     

     

    Lucie