Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog 1958 Turntable from the Black Forest - 18: Sending Files to SAMA5D4 over USB
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
  • Author Author: Jan Cumps
  • Date Created: 16 May 2015 11:29 AM Date Created
  • Views 1223 views
  • Likes 2 likes
  • Comments 2 comments
  • terminal
  • xmodem
  • enchanted_player
  • enchanted_objects
  • linux
Related
Recommended

1958 Turntable from the Black Forest - 18: Sending Files to SAMA5D4 over USB

Jan Cumps
Jan Cumps
16 May 2015

image

 

 

My lab doesn't have a wired network. And that makes it difficult to develop on the SAMA5D4 Xplained Ultra board.

The only way I am able to move compiled binaries from my Windows development machine to the board is via SCP.

But that meant that I have to connect the board to the wired network in my living room.

 

In this post you can read my successful work to enable file transfer over the USB connection. I can now transfer my programs to the board in my lab.

No need to take it out of the circuit under construction anymore.

 

image

 

Tera Term: Terminal Program with File Transfer

 

Tera Term is a terminal program, comparable to PuTTY and HyperTerminal. It has file transfer capabilities, and supports multiple protocols.

The  modus operandi isn't difficult. You first log on to the board with the serial port, similar to PuTTY.

Once connected, you have to adapt the Serial Port attributes for the Xplained Ultra.

 

image

 

Most likely this can be set in a configuration file, but I haven't looked into that yet.

On the linux prompt, log on as root.

 

Start the XMODEM listener

Prepare your linux session for file receiving by entering the rz command:

 

rz -e -b -X HelloARMWorld

 

rz is the file receive command.

-e takes care that all special commands are properly escaped

-b does a like for like (binary) transfer

-X selects the XMODEM protocol

 

Send the file

On the Tera Term menu, select File -> Transfer -> XMODEM -> Send...

image

 

A dialog pops up to select the source file. Once you selected the file, a progress bar appears:

 

image

 

When that transfer is finished, the file is available on linux.

The only thing we have to do is make it executable:

chmod +x HelloARMWorld

and run it:

./HelloARMWorld

 

image

 

Done !

 

 

Table of Contents
Chapter 1: Fix the turntable
1: Perpetuum Ebner Musical 1
2: A Time to Kill and a Time to Heal
3: Preparation for Motor Drive
4: Motor control with Infineon Motor Shield and Arduino UNO
5: Turntable speed sample testbed with Arduino UNO
6: Turntable Speed Sensor design
7: Control Theory - End of Chapter 1
Chapter 2: First Enchantments
8: Digital Light Organ Enchantment
9: Autonomous Servo Lift
10: SMD Time - Solder the IR Speed Sensor PCB
11: Yelp - who can Help me to Compile and Run my First SAMA5D4 C Program
12: Son et Lumiere - End of Chapter 2
Chapter 3: Taming the Board
13: Breakthrough - Run my own C++ Program on the SAMA5D4
14: Digital Light Organ Input Buffer
15: SAMA5D4 Blinky
16: Scope Creep
17: Audio Sampling with 16-bit ADC ADS8343
18: Sending Files to SAMA5D4 over USB
19: Port my Light Organ from Arduino to SAMA5D4
20: Fast Fourier Transform on the SAMA5D4 - End of Chapter 3
Epilogue: Reaching for the Clouds
21: Right-Sizing my Plans
22: My Own C++ Buffered Sampler on the SAMA5D4
Interlude
23: Building In the Motorized Light Organ
24: Up to the Clouds with Yún
25: Publish or Perish
26: Turntable Finished
Stretch & Boni
Bonus 1a: Remote Light Organ with WiFI pt. 1
Bonus 1b: Remote Light Organ with WiFI pt. 2
Grande Finale: Paho MQTT Client on the SAMA5D4
Related blog
Vintage Turntable repair: Can I fix a Perpetuum Ebner from 1958
Review 1: Atmel SMART SAMA5D4 Xplained Ultra Unboxing and First Steps
Review 2: Atmel SMART SAMA5D4 Xplained Ultra - Building the Libraries from Source
Review 3: Digital Continuous Rotation (360°) Servo Part 1
Review 4: Digital Continuous Rotation (360°) Servo Part 2
Review 5: Atmel SMART SAMA5D4 Xplained Ultra - TCP/IP running
Review 6: Atmel SMART SAMA5D4 Xplained Ultra - LINUX Distro with SSH support
poem
Enchanted Objects: Let's work together to tame the ATMEL SMART SAMA5D4 Xplained Ultra kit
17 bis: Off South...
Review 7: Atmel SMART SAMA5D4 Xplained Ultra - C++ ADC Example on Linux
Review 8: Atmel SMART SAMA5D4 Xplained Ultra - Product Review
Review 9a: Atmel SMART SAMA5D4 Xplained Ultra - Set up ADC Buffer with Hardware Trigger Part 1
Review 9b: Atmel SMART SAMA5D4 Xplained Ultra - Set up ADC Buffer with Hardware Trigger Part 2
Review 10: Atmel SMART SAMA5D4 Xplained Ultra - New Content on AT91.com
1958 Turntable from the Black Forest - Summary of the Enchanted Player Story
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 11 years ago +2
    Finally got my first c++ program running that samples analog signal:
  • Jan Cumps
    Jan Cumps over 11 years ago

    Finally got my first c++ program running that samples analog signal:

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 11 years ago

    I tried to attach the HelloARMWorld binary for those who want to play along @home.

    But binaries are a restricted filetype, and I don't want to play the system by faking that it isn't a binary.


    Send me a PM with your email address if you want to try this out with this binary.

    Alternatively, check 1958 Turntable from the Black Forest - 13: Breakthrough - Run my own C++ Program on the SAMA5D4