FPGA
  • Technologies
  • More
FPGA
Blog Automate Repeatable Steps in Vivado
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 12 Aug 2021 10:39 AM Date Created
  • Views 5416 views
  • Likes 11 likes
  • Comments 6 comments
  • summer_of_fpgas
  • summer of fpgas
Related
Recommended

Automate Repeatable Steps in Vivado

Jan Cumps
Jan Cumps
12 Aug 2021

Life hack to automate the creation of a project in Vivado.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

video source: real time capture of script execution on my laptop

 

Many projects have repeatable steps at the setup stage. This script helps to automate this. It creates a new project with your typical starting blocks.

Before calling the script, close the currect project, if one is open.

If you just opened Vivado, you are good to go. The Tcl prompt is at the bottom of the startup screen.

Set these two properties using that prompt. The Vivado project will be created with that name and location you define here.

 

set projectname myProject
set projectroot D:/users/jancu/Documents/elektronica/xilinx/zynq/prj

 

TCL script:

gist: https://gist.github.com/jancumps/a10e0395fe37c70e8d90fdba1ebae948#file-create_project-tcl

 

create_project $projectname $projectroot/$projectname -part xc7z020clg400-1
set_property board_part tul.com.tw:pynq-z2:part0:1.0 [current_project]
set_property target_language VHDL [current_project]

create_bd_design "design_1"
startgroup
create_bd_cell -type ip -vlnv xilinx.com:ip:processing_system7:5.5 processing_system7_0
endgroup
startgroup
create_bd_cell -type ip -vlnv xilinx.com:ip:proc_sys_reset:5.0 proc_sys_reset_0
endgroup
startgroup
create_bd_cell -type ip -vlnv xilinx.com:ip:axi_interconnect:2.1 axi_interconnect_0
endgroup
startgroup
set_property -dict [list CONFIG.NUM_MI {1}] [get_bd_cells axi_interconnect_0]
endgroup
startgroup
create_bd_cell -type ip -vlnv xilinx.com:ip:axi_gpio:2.0 axi_gpio_0
endgroup
apply_bd_automation -rule xilinx.com:bd_rule:processing_system7 -config {make_external "FIXED_IO, DDR" apply_board_preset "1" Master "Disable" Slave "Disable" }  [get_bd_cells processing_system7_0]
connect_bd_net [get_bd_pins processing_system7_0/FCLK_CLK0] [get_bd_pins processing_system7_0/M_AXI_GP0_ACLK]
connect_bd_net [get_bd_pins axi_interconnect_0/ACLK] [get_bd_pins processing_system7_0/FCLK_CLK0]
connect_bd_net [get_bd_pins axi_interconnect_0/S00_ACLK] [get_bd_pins processing_system7_0/FCLK_CLK0]
connect_bd_net [get_bd_pins axi_interconnect_0/M00_ACLK] [get_bd_pins processing_system7_0/FCLK_CLK0]
connect_bd_net [get_bd_pins proc_sys_reset_0/slowest_sync_clk] [get_bd_pins processing_system7_0/FCLK_CLK0]
connect_bd_net [get_bd_pins processing_system7_0/FCLK_RESET0_N] [get_bd_pins proc_sys_reset_0/ext_reset_in]
connect_bd_net [get_bd_pins proc_sys_reset_0/interconnect_aresetn] [get_bd_pins axi_interconnect_0/ARESETN]
connect_bd_net [get_bd_pins proc_sys_reset_0/peripheral_aresetn] [get_bd_pins axi_interconnect_0/S00_ARESETN]
connect_bd_net [get_bd_pins axi_interconnect_0/M00_ARESETN] [get_bd_pins proc_sys_reset_0/peripheral_aresetn]
connect_bd_net [get_bd_pins axi_gpio_0/s_axi_aclk] [get_bd_pins processing_system7_0/FCLK_CLK0]
connect_bd_net [get_bd_pins axi_gpio_0/s_axi_aresetn] [get_bd_pins proc_sys_reset_0/peripheral_aresetn]
connect_bd_intf_net [get_bd_intf_pins axi_gpio_0/S_AXI] -boundary_type upper [get_bd_intf_pins axi_interconnect_0/M00_AXI]
connect_bd_intf_net [get_bd_intf_pins processing_system7_0/M_AXI_GP0] -boundary_type upper [get_bd_intf_pins axi_interconnect_0/S00_AXI]
save_bd_design

 

image

image source: screen capture of the block design after the script finished

 

The script

  • sets the correct device (for my Pynq-Z2. If you have another board, create one project manually and harvest the steps from the Tcl log)
  • creates a project and a block design
  • adds the Zynq PS and applies board presets
  • adds reset and AXI IPs
  • connects and saves.
  • is tested with Vivado 2020.2, but doesn't use version specific constructs.

voila.

 

 

Pynq - Zync - Vivado series
Add Pynq-Z2 board to Vivado
Learning Xilinx Zynq: port a Spartan 6 PWM example to Pynq
Learning Xilinx Zynq: use AXI with a VHDL example in Pynq
VHDL PWM generator with dead time: the design
Learning Xilinx Zynq: use AXI and MMIO with a VHDL example in Pynq
Learning Xilinx Zynq: port Rotary Decoder from Spartan 6 to Vivado and PYNQ
Learning Xilinx Zynq: FPGA based PWM generator with scroll wheel control
Learning Xilinx Zynq: use RAM design for Altera Cyclone on Vivado and PYNQ
Learning Xilinx Zynq: a Quadrature Oscillator - 2 implementations
Learning Xilinx Zynq: a Quadrature Oscillator - variable frequency
Learning Xilinx Zynq: Hardware Accelerated Software
Automate Repeatable Steps in Vivado
Learning Xilinx Zynq: Try to make my own Accelerated OpenCV Function - 1: Vitis HLS
Learning Xilinx Zynq: Try to make my own Accelerated OpenCV Function - 2: Vivado Block Design
Learning Xilinx Zynq: Logic Gates in Vivado
Learning Xilinx Zynq: Interrupt ARM from FPGA fabric
Learning Xilinx Zynq: reuse and combine components to build a multiplexer
PYNQ version 2.7 (Austin) is released
PYNQ and Zynq: the Vitis HLS Accelerator with DMA training - Part 1: Turn C++ code into an FPGA IP
PYNQ and Zynq: the Vitis HLS Accelerator with DMA training - Part 2: Add the Accelerated IP to a Vivado design
PYNQ and Zynq: the Vitis HLS Accelerator with DMA training - Part 3: Use the Hardware Accelerated Code in Software
PYNQ and Zynq: the Vitis HLS Accelerator with DMA training - Deep Dive: the data streams between Accelerator IP and ARM processors
Use the ZYNQ XADC with DMA part 1: bare metal
Use the ZYNQ XADC with DMA part 2: get and show samples in PYNQ
VHDL: Convert a Fixed Module into a Generic Module for Reuse
  • Sign in to reply

Top Comments

  • Andrew J
    Andrew J over 5 years ago +2
    Nice. I worked out yesterday that the TCL console shows the actual commands being executed as you 'do stuff' in Vivado. Great idea to scriptify.
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to Andrew J +2
    Andrew J wrote: ... the TCL console shows the actual commands being executed as you 'do stuff' in Vivado. ... That is how I captured the commands for this article. I played the creation of a project in…
  • Jan Cumps
    Jan Cumps over 5 years ago +2
    some random commands I've used recently, to visualise selected objects for blogs: highlight_objects -color blue [get_bd_cells /timer_0] highlight_objects -color blue [get_bd_cells /timer_*] highlight_objects…
Parents
  • bhfletcher
    bhfletcher over 5 years ago

    Great work! Thank you for showcasing this. Avnet's more advanced projects take advantage of Tcl scripting, so it is well worth the time to understand Vivado Tcl capabilities. If you want to see some of Avnet's examples, this blog by narrucmot will share where to find Avnet's scripts on GitHub.

    Avnet HDL git HOWTO (Vivado 2020.2 and later)

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • bhfletcher
    bhfletcher over 5 years ago

    Great work! Thank you for showcasing this. Avnet's more advanced projects take advantage of Tcl scripting, so it is well worth the time to understand Vivado Tcl capabilities. If you want to see some of Avnet's examples, this blog by narrucmot will share where to find Avnet's scripts on GitHub.

    Avnet HDL git HOWTO (Vivado 2020.2 and later)

     

    Bryan