Power & Energy
  • Technologies
  • More
Power & Energy
Blog
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • ANDRITZ is Replacing the Old Hickory Dam Equipment

    Catwell
    Catwell
    The Old Hickory Dam is being upgraded with a 7-blade turbine and new runners. (Image Credit: Mark Rankin/US Army Corps of Engineers) Big projects usually don’t finish when first expected. At Tennessee’s Old Hickory Dam, ANDRITZ was suppo...
    • 18 Sep 2026
  • Farmers in Egypt Use Solar Panels to Grow Crops

    Catwell
    Catwell
    Agrovoltaics. (Image Credit: ADMC/pixabay) For thousands of years, Egypt has made agriculture work in its harsh environment. Nowadays, however, farmers are facing more challenges: water scarcity and increasing temperatures that damage crops. Agrovo...
    • 17 Sep 2026
  • Scientists Created Batteries Made of Chitosan from Seafood Waste

    Catwell
    Catwell
    (Image Credit: Chandler Cruttenden/Unsplash) Poor crabs. Aqueous zinc-metal batteries could be applicable for grid storage. After all, there is a lot of zinc, and it’s cheaper and safer than lithium. Conventional liquid electrolytes and polyme...
    • 16 Sep 2026
  • NASA Plans to Launch a Nuclear Reactor in Space

    Catwell
    Catwell
    Artist’s concept of the Space Reactor-1 Freedom spacecraft flying past Mars. (Image Credit: NASA) Solar power can be limited for deep space travel. When spacecraft move farther away from the sun, the sunlight reaching their solar panel weakens...
    • 4 Sep 2026
  • Researchers Create Digital Twin of a Battery to Uncover What Causes Degradation During Fast Charging

    Catwell
    Catwell
    Diagram of the team’s research. (Image Credit: Kang et al., InfoMat 2026. Creative Commons Attribution License) Fast charging cuts down on lithium-ion batteries charging time. However, transporting the lithium into electrodes at high rates le...
    • 1 Sep 2026
  • AI Data Centers Require a Lot of Water, Where Does It Go?

    Catwell
    Catwell
    AI data centers use water to cool the servers. (Image Credit: UCR/Evan Fields) I was wondering why water used in data centers can’t be reused. Nature cycles water constantly, it seems odd that the water is used to cool but then disappears. Why...
    • 7 Aug 2026
  • Honeycomb-Shaped 3D PV Modules Could Generate More Electricity Than Flat Panels

    Catwell
    Catwell
    Figure showing the honeycomb-structured 3D PV design, the mechanical metamaterial support, and the light recapture mechanism. (Image Credit: Advanced Materials Technologies) Although PV modules are useful, they have a flaw. They don’t retain a...
    • 31 Jul 2026
  • Ancient Cities Are Now Using Solar Panels in Roof Tiles

    Catwell
    Catwell
    Roof tiles in the Villa of the Mysteries produce power. (Image Credit: Pompeii Archaeological Park) Renewables in ancient cities? While solar panels produce clean energy, there’s usually a catch. The problem? Solar panels affect the appearance...
    • 10 Jul 2026
  • MIT Develops a New Technique to Extract Lithium from Spodumene Rock

    Catwell
    Catwell
    (Image Credit: Wikimedia Commons) MIT researchers recently created a new method to extract lithium from spodumene rock using a low-temperature process. A bathroom renovation inspired the research. At the time, Yet-Ming Chiang, MIT’s Kyocera Pr...
    • 12 Jun 2026
  • Researchers Develop Water Battery That Can Be Safely Disposed

    Catwell
    Catwell
    Comparing the neutral pH 7 with other battery technologies. (Image Credit: nature) Researchers at the City University of Hong Kong have developed an aqueous battery with a pH 7 electrolyte. The battery system is built with water-based materials and ...
    • 21 May 2026
  • A Modeling Study Predicts That Solar Farms Could Produce Rainfall

    Catwell
    Catwell
    A solar farm. (Image Credit: TheOtherKev/pixabay) Is that bad? In the UAE, where water is harder to come by than oil, cloud seeding or desalination plants produce freshwater for everyone living there. Now, a 2024 modeling study says huge solar farms...
    • 24 Apr 2026
  • Deep Fission is Burying Nuclear Reactors One Mile Deep

    Catwell
    Catwell
    Deep Fission is a startup focusing on the burial of nuclear reactors as a cheaper, simpler alternative to traditional above-ground power plants. (Image Credit: Deep Fission) Nuclear power is becoming more complex and costly, and one startup wants to...
    • 8 Apr 2026
  • Engineers Build a Alt Energy Device That Generates Power at Night

    Catwell
    Catwell
    Render and data show radiative cooling of the top plate to the night sky and warming of the bottom plate to the ground. This produced a temperature difference that powered the engine. (Image Credit: ScienceAdvances) Engineers at the University ...
    • 4 Mar 2026
  • Japan’s Sidewalks Converts Human Footsteps into Useable Electricity

    Catwell
    Catwell
    (Image Credit: Wikimedia Commons) Wind and sunlight are the most common sources of renewable energy, powering turbines and solar panels worldwide. Japan and other countries are now tapping a subtler source: footsteps on piezoelectric sidewalks to ge...
    • 3 Mar 2026
  • Japan is Working on Three Surprising Hydrogen Projects

    Catwell
    Catwell
    Rendering of the co-firing hydrogen engine built by Kawasaki Heavy Industries. (Image Credit: Kawasaki) Kawasaki Heavy Industries constructed the first-ever 8MW KG Series co-firing hydrogen engine, which generates electricity. It operates on natural...
    • 20 Feb 2026
  • Japan Extracts Rare Earth Elements from Seabed Mud

    Catwell
    Catwell
    Japan’s Chikyu deep-sea drilling vessel recently extracted samples of rare earth elements from seabed sediment. (Photo By Gleam - Photo taken by Gleam., CC BY-SA 3.0) Japan is starting to take action on a decade-old plan to move away from Chi...
    • 9 Feb 2026
  • Energy left in "dead" batteries?!

    Attila Tőkés
    Attila Tőkés
    Hi Element14 Community!  Traditional alkaline batteries tend to "die" at the most inconvenient times. I used to I have them in devices like wireless mouse and keyboards, and it felt that the batteries were draining fairly quickly, catc...
    • 1 Feb 2026
  • Building a Smart Electronic Load | 2026 Update (#3)

    Attila Tőkés
    Attila Tőkés
    Hi E14 Community!  Wanted to give a quick update on my Smart Electronic Load project. Since the last time from one year ago, Building a Smart Electronic Load | DAC and Initial Firmware (#2), the project was progressing relati...
    • 18 Jan 2026
  • Triplet Antennas Unlock Low-Voltage NIR-II LEDs

    Catwell
    Catwell
    Artist’s rendering of a lanthanide-doped nanoparticle in the shape of a spider and the web (made of 9-ACA). (Image Credit: Zhongzheng Yu/) Engineers at the University of Cambridge have developed a technique that enables the electrical activati...
    • 30 Dec 2025
  • Hot Gadget Alert: My First Tinker With the Multicomp Pro Thermal Camera

    foxbat
    foxbat
    Unboxing the Multicomp Pro Professional Thermal Imager : A First Look The fine (and clearly very patient) folks of the element14 Community somehow concluded that my particular brand of Halloween-themed tinkering deserved to win this year’s Hall...
    • 19 Dec 2025
  • Designing for Ultra-Low Power: Strategies for Edge and Battery-Powered Devices

    Catwell
    Catwell
      (Image credit: Pixabay) If you’ve ever designed a product meant to run off a battery and last a long time, you know how brutal reality can be. You start with hope and a 10,000 mAh battery, and six months later, you’re back in meeti...
    • 18 Dec 2025
  • Researchers Develop Energy Harvesting System That Could Power Wearables

    Catwell
    Catwell
    The IE-TENG system generates electricity through the intrusion and extrusion of liquid in the silicon nanopores. (Image Credit: TU Hamburg, DESY, Künsting) Engineers at Hamburg University of Technology (TUHH) and other European institutions dev...
    • 9 Dec 2025
  • Inventor of the Super Soaker is Working on a Next Gen Energy Generation Device

    Catwell
    Catwell
    Lonnie Johnson, inventor of the Super Soaker, is working on the JTEC device. (Image Credit: Johnson Energy Storage) We’re familiar with the legendary Super Soaker, a fun water gun invented by Lonnie Johnson that earned him a $1 billion profit ...
    • 5 Dec 2025
  • The Latest Insight into Low-Power Design for Always-On Edge AI Devices

    Catwell
    Catwell
    (Image credit: Freepik) AI is no longer limited to cloud data centers or high-performance machines; it’s being pushed to the edge in the form of mobile devices, smart cameras, industrial sensors, wearables, and other consumer platforms. These ...
    • 21 Nov 2025
  • The Rise of GaN and SiC: What Power Designers Need to Know

    Catwell
    Catwell
    (Image credit: Pixabay) For years, silicon has been the default foundation of power electronics, but like any technology, that’s changing fast. Wide-bandgap semiconductors such as Gallium Nitride (GaN) and Silicon Carbide (SiC) are transformin...
    • 18 Nov 2025
>