FPGA
  • Technologies
  • More
FPGA
Blog Add Pynq-Z2 board to Vivado
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 31 May 2021 7:47 PM Date Created
  • Views 39253 views
  • Likes 13 likes
  • Comments 40 comments
  • zynq
  • xilinx
  • jupyter
  • fpga
  • vivado
  • pynq
Related
Recommended

Add Pynq-Z2 board to Vivado

Jan Cumps
Jan Cumps
31 May 2021

Instructions on how to add the Pynq-Z2Pynq-Z2 board to Vivado.

This allows you to create projects and custom FPGA bit streams for it.

 

image

image source: customer action video after completing the instruction video of Cathal McCabe listed at the end of this post.

 

In the Vivado project creation wizard, there is a possibility to prime your design from a board definition.

You don't need to find out what the exact FPGA is, and what hardware is available.

There are more project preparation tools. Constraint files and TCL files that fully define the board with all possibilities enabled.

This post focuses on the board definition.

image

 

Get the board file

 

The files listed on pync.io are not available. I found them here.

image

 

Install and register the board in Vivado

 

Then there are two options.

  • (deprecated) Directly put the files in the Vivado boards folder: <Xilinx installation directory>\Vivado\<version>\data\boards\board_files.
  • Or (preferred)  put them at a location you decide, and add a line to the Vivado init file, %APPDATA%/Xilinx/Vivado/init.tcl (create it if it does not exist)
    set_param board.repoPaths [list "D:/Xilinx/pynq-z2/A.0"]

I used the 2nd option. You have to restart the editor.

 

The result is that you can now create projects that have the right FPGA info for the Pynq-Z2:

image

 

My goal for this week is to replicate this exercise from Cathal McCabe from the Pynq community:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

I attached the project to this post, and the jupyter notebook.

I changed some things:

32 bit GPIO instead of 64

A reset input for the Johnson Counter module

Translated the Verilog Counter code to VHDL.

 

 

Pynq - Zync - Vivado series
Add Pynq-Z2 board to Vivado
Learning Xilinx Zynq: port a Spartan 6 PWM example to Pynq
Learning Xilinx Zynq: use AXI with a VHDL example in Pynq
VHDL PWM generator with dead time: the design
Learning Xilinx Zynq: use AXI and MMIO with a VHDL example in Pynq
Learning Xilinx Zynq: port Rotary Decoder from Spartan 6 to Vivado and PYNQ
Learning Xilinx Zynq: FPGA based PWM generator with scroll wheel control
Learning Xilinx Zynq: use RAM design for Altera Cyclone on Vivado and PYNQ
Learning Xilinx Zynq: a Quadrature Oscillator - 2 implementations
Learning Xilinx Zynq: a Quadrature Oscillator - variable frequency
Learning Xilinx Zynq: Hardware Accelerated Software
Automate Repeatable Steps in Vivado
Learning Xilinx Zynq: Try to make my own Accelerated OpenCV Function - 1: Vitis HLS
Learning Xilinx Zynq: Try to make my own Accelerated OpenCV Function - 2: Vivado Block Design
Learning Xilinx Zynq: Logic Gates in Vivado
Learning Xilinx Zynq: Interrupt ARM from FPGA fabric
Learning Xilinx Zynq: reuse and combine components to build a multiplexer
PYNQ version 2.7 (Austin) is released
PYNQ and Zynq: the Vitis HLS Accelerator with DMA training - Part 1: Turn C++ code into an FPGA IP
PYNQ and Zynq: the Vitis HLS Accelerator with DMA training - Part 2: Add the Accelerated IP to a Vivado design
PYNQ and Zynq: the Vitis HLS Accelerator with DMA training - Part 3: Use the Hardware Accelerated Code in Software
PYNQ and Zynq: the Vitis HLS Accelerator with DMA training - Deep Dive: the data streams between Accelerator IP and ARM processors
Use the ZYNQ XADC with DMA part 1: bare metal
Use the ZYNQ XADC with DMA part 2: get and show samples in PYNQ
VHDL: Convert a Fixed Module into a Generic Module for Reuse
Attachments:
johnson_counter.zip
johnson_counter_jupyter_notebook.zip
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 5 years ago +2
    So far so good ...
  • narrucmot
    narrucmot over 5 years ago in reply to Jan Cumps +2
    Very cool! Glad you got this working! --Tom
  • drozwood90
    drozwood90 over 5 years ago in reply to Jan Cumps +2
    Hi Jan, Can I offer a suggestion? Please bold " set_param board.repoPaths [list "D:/Xilinx/pynq-z2/A.0"]" That is something that so many people miss. That is really the proper way that Xilinx suggests…
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to kk10

    navadeepganeshu  wrote:

     

    I am at this point now. Taking 1hr+ to synthesize this design image

    That project is a treasure. Next to the traditional FPGA thingies, it has 4 MicroBlaze soft controllers (one for the Arduino, one for the RaspBerry Pi, and one for each PMOD connector), SPI and I2C IPs, ...

    It's also useful to check out the Base Overlay python code to see how they are building a library around this. It helps to understand the Jupyter Base examples better.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • navadeepganeshu
    navadeepganeshu over 5 years ago in reply to Jan Cumps

    I am at this point now. Taking 1hr+ to synthesize this design image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to kk10

    Can you check if you saved the init.tcl file as ascii / UTF-8 or UNICODE 16?

    If the file has a size of +- 50 bytes, it is OK. If it has 100+ bytes, it's most likely saved as UNICODE 16.

    In that case, it's possible that Vivado stumbles over the double quotes.

    If you used notepad or notepad+ to generate it, validate that the output is set to ascii or UTF-8 wile saving.

     

    Then, after startup, check what the TCL console (available at the bottom of the Vivado screen)  says.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to Jan Cumps

    Both builds were successful.

    image

     

     

    instructions:

    clone https://github.com/Xilinx/PYNQ

     

    Start Vivado 2020.1 Tcl Shell

     

    cd PYNQ/boards/Pynq-Z2

     

    base:

    cd base
    exec vivado -mode batch -source build_ip.tcl -notrace
    exec vivado -mode batch -source base.tcl -notrace
    exec vivado -mode batch -source build_bitstream.tcl -notrace
    exec vivado -mode batch -source check_timing.tcl -notrace

     

    cd ..

     

    logictools:

    cd logictools
    exec vivado -mode batch -source build_ip.tcl -notrace
    exec vivado -mode batch -source logictools.tcl -notrace
    exec vivado -mode batch -source build_bitstream.tcl -notrace
    exec vivado -mode batch -source check_timing.tcl -notrace

     

    That's it. You now have two projects and the .bit and .hwh files.

    Don't open the projects in the Vivado IDE before you generated the bitstream via TCL. Otherwise the wrapper and top level file aren't set.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago

    I installed Vivado 2020-1 now, to recreate the base and logictools designs.

    image

     

    First step is to generate the IP. So far so good:

    image

     

    Creating the project worked:

    Vivado% exec vivado -mode batch -source base.tcl -notrace

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>