FPGA
  • Technologies
  • More
FPGA
Blog Add Pynq-Z2 board to Vivado
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 31 May 2021 7:47 PM Date Created
  • Views 39241 views
  • Likes 13 likes
  • Comments 40 comments
  • zynq
  • xilinx
  • jupyter
  • fpga
  • vivado
  • pynq
Related
Recommended

Add Pynq-Z2 board to Vivado

Jan Cumps
Jan Cumps
31 May 2021

Instructions on how to add the Pynq-Z2Pynq-Z2 board to Vivado.

This allows you to create projects and custom FPGA bit streams for it.

 

image

image source: customer action video after completing the instruction video of Cathal McCabe listed at the end of this post.

 

In the Vivado project creation wizard, there is a possibility to prime your design from a board definition.

You don't need to find out what the exact FPGA is, and what hardware is available.

There are more project preparation tools. Constraint files and TCL files that fully define the board with all possibilities enabled.

This post focuses on the board definition.

image

 

Get the board file

 

The files listed on pync.io are not available. I found them here.

image

 

Install and register the board in Vivado

 

Then there are two options.

  • (deprecated) Directly put the files in the Vivado boards folder: <Xilinx installation directory>\Vivado\<version>\data\boards\board_files.
  • Or (preferred)  put them at a location you decide, and add a line to the Vivado init file, %APPDATA%/Xilinx/Vivado/init.tcl (create it if it does not exist)
    set_param board.repoPaths [list "D:/Xilinx/pynq-z2/A.0"]

I used the 2nd option. You have to restart the editor.

 

The result is that you can now create projects that have the right FPGA info for the Pynq-Z2:

image

 

My goal for this week is to replicate this exercise from Cathal McCabe from the Pynq community:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

I attached the project to this post, and the jupyter notebook.

I changed some things:

32 bit GPIO instead of 64

A reset input for the Johnson Counter module

Translated the Verilog Counter code to VHDL.

 

 

Pynq - Zync - Vivado series
Add Pynq-Z2 board to Vivado
Learning Xilinx Zynq: port a Spartan 6 PWM example to Pynq
Learning Xilinx Zynq: use AXI with a VHDL example in Pynq
VHDL PWM generator with dead time: the design
Learning Xilinx Zynq: use AXI and MMIO with a VHDL example in Pynq
Learning Xilinx Zynq: port Rotary Decoder from Spartan 6 to Vivado and PYNQ
Learning Xilinx Zynq: FPGA based PWM generator with scroll wheel control
Learning Xilinx Zynq: use RAM design for Altera Cyclone on Vivado and PYNQ
Learning Xilinx Zynq: a Quadrature Oscillator - 2 implementations
Learning Xilinx Zynq: a Quadrature Oscillator - variable frequency
Learning Xilinx Zynq: Hardware Accelerated Software
Automate Repeatable Steps in Vivado
Learning Xilinx Zynq: Try to make my own Accelerated OpenCV Function - 1: Vitis HLS
Learning Xilinx Zynq: Try to make my own Accelerated OpenCV Function - 2: Vivado Block Design
Learning Xilinx Zynq: Logic Gates in Vivado
Learning Xilinx Zynq: Interrupt ARM from FPGA fabric
Learning Xilinx Zynq: reuse and combine components to build a multiplexer
PYNQ version 2.7 (Austin) is released
PYNQ and Zynq: the Vitis HLS Accelerator with DMA training - Part 1: Turn C++ code into an FPGA IP
PYNQ and Zynq: the Vitis HLS Accelerator with DMA training - Part 2: Add the Accelerated IP to a Vivado design
PYNQ and Zynq: the Vitis HLS Accelerator with DMA training - Part 3: Use the Hardware Accelerated Code in Software
PYNQ and Zynq: the Vitis HLS Accelerator with DMA training - Deep Dive: the data streams between Accelerator IP and ARM processors
Use the ZYNQ XADC with DMA part 1: bare metal
Use the ZYNQ XADC with DMA part 2: get and show samples in PYNQ
VHDL: Convert a Fixed Module into a Generic Module for Reuse
Attachments:
johnson_counter.zip
johnson_counter_jupyter_notebook.zip
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 5 years ago +2
    So far so good ...
  • narrucmot
    narrucmot over 5 years ago in reply to Jan Cumps +2
    Very cool! Glad you got this working! --Tom
  • drozwood90
    drozwood90 over 5 years ago in reply to Jan Cumps +2
    Hi Jan, Can I offer a suggestion? Please bold " set_param board.repoPaths [list "D:/Xilinx/pynq-z2/A.0"]" That is something that so many people miss. That is really the proper way that Xilinx suggests…
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to kk10

    Use forward slashes in the text file, as per instructions.

    You use \  It should be /

     

    Also, you do not have part of the start of the line.

    Yours starts with ram. The instructions say to start with set_param.

     

    Also, you do not have the full path. The files are in pynq-z2/A.0 not in pynq-z2.

     

    My general advise is to stick to the instructions. It will help you with every next step on your path to master the Zynq.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kk10
    kk10 over 5 years ago in reply to Jan Cumps

    C:\Users\Lenovo\AppData\Roaming-APPDATA directory

    image

    imageimageimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to kk10

    If the instructions above do not work for you, please contact Xilinx.

    I got the instructions from them. I followed them step by step, and it worked.

    If you also did the same, literally followed each and every step,  and it does not work, Xilinx support should be your next step.

     

    Alternatively you could:

    show us where your %APPDATA% directory is. (feedback)

    show us a directory listing of that directory. (feedback)

    show us the exact content of the init.tcl file in that directory (feedback)

    show us where you extracted the board info archive. (feedback)

    show us a directory listing of that directory (feedback)

    stop Vivado if it is running

    start Vivado

    show us what you see/don't see when you create a new project. (feedback)

     

    3rd alternative: do not follow my instructions but use the original ones: https://www.xilinx.com/support/answers/72033.html

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kk10
    kk10 over 5 years ago in reply to Jan Cumps

    I have created a text file. Is that sufficient?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to kk10

    kk10  wrote:

     

    I found the directory. Thank you. I have copied the extracted file into the first link which you specified. Yet when i open Vivado that board isn't visible. Kindly help me with this

     

    add a line to the Vivado init file called init.tcl, that is either already located in  %APPDATA%/Xilinx/Vivado, or does not exist. In the case that it does not exist create a file called init.tcl there.

     

    %APPDATA% is a windows directory.

    You can find it by opening a command prompt and typing:

    echo %APPDATA%

     

    The result will show the location. In my case:

    C:\Users\jancu\AppData\Roaming

     

    The line you add or enter to that file should look like this:

    set_param board.repoPaths [list "D:/Xilinx/pynq-z2/A.0"]

     

    Where I show D:/Xilinx/pynq-z2/A.0, you should put the directory where you placed  the extracted files.

     

    It is the directory that contains these files, if you extracted the correct archive:

    Directory of D:\Xilinx\pynq-z2\A.0
    30-05-2018  19:19            54 479 board.xml
    27-06-2018  00:14             9 007 part0_pins.xml
    19-06-2018  07:48            74 492 preset.xml
    27-06-2018  04:48           175 776 pynq_z2.jpg

     

    Do not deviate from the steps. Use forward slashes, as specified in the article I linked in.

    Restart Vivado, if it was already running.

    If this does not work, I suggest you contact Xilinx support. I do not know how to fix it if it does not work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>