FPGA
  • Technologies
  • More
FPGA
Blog
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join FPGA to participate - click to join for free!

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Vitis-AI 1.4 Flow for Avnet Vitis platforms

    albertabeef
    albertabeef
    Avnet is working on Vitis 2021.1 platforms for several of their hardware platforms.Thanks to this work, I was able to port Vitis-AI 1.4 on the following platforms:Ultra96-V2 Development BoardUltraZed-EV SOM (7EV) + FMC Carrier CardUltraZed-EG SOM (3E...
    • 20 Oct 2021
  • The Art of FPGA Design - Post 37

    fpgaguru
    fpgaguru
    Recent Advances in Vivado VHDL-2008 Support   Previous posts in this blog were made in the 2018-2019 period. Some of the issues presented were an attempt to work around VHDL-2008 support limitations in Vivado at that point in time. Since then, s...
    • 3 Oct 2021
  • 3 Tips You Should Know Before Developing a Xilinx PCB

    bhfletcher
    bhfletcher
    Our team at Avnet is working on a new design now. As we go through the various review stages, I was reminded of something that every engineer developing a PCB with Xilinx should know. Tip #1 -- Use Xilinx Documentation NavigatorOf course, every ...
    • 29 Sep 2021
  • Learning Xilinx Zynq: reuse and combine components to build a multiplexer

    Jan Cumps
    Jan Cumps
    Build a big multiplexer by reusing small multiplexers. FPGA designs are (re)usable as components. In this post I'm showing that you can make a 4-input multiplexer by combining several 2-input multiplexers. A 2-input multiplexer is a simple digita...
    • 14 Sep 2021
  • Learning Xilinx Zynq: Interrupt ARM from FPGA fabric

    Jan Cumps
    Jan Cumps
    You can interrupt the Zynq ARM side with a signal coming out of the FPGA part of the chip. In this post, I test this. The FPGA part has a few blocks that will generate interrupts. In a Jupyter notebook, I'll try to show that they are detected by the ...
    • 5 Sep 2021
  • Ultra96-V2 Dual Camera Design for 2020.2

    albertabeef
    albertabeef
    IntroductionThis blog post provides details on how to build and execute the new 2020.2 design for the Ultra96-V2 development board with Dual-Camera Mezzanine.  {gallery} Ultra96-V2 Dual Camera PhotosUltra96-V2 with Dual Camera MezzanineUltr...
    • 3 Sep 2021
  • Learning Xilinx Zynq: a Quadrature Oscillator - variable frequency

    Jan Cumps
    Jan Cumps
    This post is a follow up on a previous article to generate a quadrature clock for shabaz 's Software Defined Radio (SDR) Experiment Board. It's a circuit with 4 PWM outputs that are each 90° shifted. I'm adding programmable frequency control. Wit...
    • 31 Aug 2021
  • Summer of FPGA, Workshop 4: Elaborating on the workshop design

    Andrew J
    Andrew J
    IntroductionWorkshop 4 of the Summer of FPGA series for the Ultra96-V2 board went through a design for using the Mezzanine Click board.  It was covered 'at pace' and this blog is my jottings on the steps taken, specifically elaborating on some o...
    • 27 Aug 2021
  • Summer of FPGA, Workshop 4: Elaborating on creating custom IP

    Andrew J
    Andrew J
    IntroductionWorkshop 4 of the Summer of FPGA series for the Ultra96-V2 board went through a design for using the Mezzanine Click board.  It was covered 'at pace' and this blog is my jottings on the steps taken, specifically elaborating o...
    • 27 Aug 2021
  • New! Avnet Boards Xilinx Solutions Guide

    narrucmot
    narrucmot
    Hello! Looking for a new Xilinx SBC to play with or the best Xilinx Zynq or Zynq UltraScale+ SOM to use in your product?  Can't decide what Avnet SOM or SBC is the best fit for your application?  Avnet has just published a new Xili...
    • 26 Aug 2021
  • Learning Xilinx Zynq: Logic Gates in Vivado

    Jan Cumps
    Jan Cumps
    When you're working on a Vivado Block design, you can add IP. There are 100s of options available. But you will not find a NOT gate, AND gate, ... They are there though, available under the cryptical name Utility Vector Logic and Utility Reduced Logi...
    • 18 Aug 2021
  • Summer of FPGAs - Building an Embedded System on FPGA

    yesha98
    yesha98
    Introduction: Back then in February when I roadtested the USB104-A7, I had learned to create block designs using MicroBlaze. I found it very interesting but the available online resources were limited, the tutorials were based on the older versions o...
    • 16 Aug 2021
  • Learning Xilinx Zynq: Try to make my own Accelerated OpenCV Function - 2: Vivado Block Design

    Jan Cumps
    Jan Cumps
    Read this for info only. The project done at the time didn't work. I'm leaving the blog here as a testimonial that things have become easier and more streamlined with the 2.7 release of the example.It works, and can easily be repeated, with Vitis HLS...
    • 16 Aug 2021
  • Learning Xilinx Zynq: Try to make my own Accelerated OpenCV Function - 1: Vitis HLS

    Jan Cumps
    Jan Cumps
    Read this for info only. The project done at  the time didn't work. I'm leaving the blog here as a testimonial that things have become easier and more streamlined with the 2.7 release of the example. It works, and can easily be repeated, with Vi...
    • 15 Aug 2021
  • Automate Repeatable Steps in Vivado

    Jan Cumps
    Jan Cumps
    Life hack to automate the creation of a project in Vivado.   www.youtube.com/watch video source: real time capture of script execution on my laptop   Many projects have repeatable steps at the setup stage. This script helps to automate this...
    • 12 Aug 2021
  • Learning Xilinx Zynq: Hardware Accelerated Software

    Jan Cumps
    Jan Cumps
    The main target for Zynq family FPGAs is: compute systems with hardware acceleration. It's architecture focuses on being able to stream data efficiently between ARM and FPGA submodules. The FPGA can then perform manipulations in hardware that tak...
    • 8 Aug 2021
  • Learning Xilinx Zynq: a Quadrature Oscillator - 2 implementations

    Jan Cumps
    Jan Cumps
    shabaz made a Software Defined Radio (SDR) Experiment Board. One of the components is a digital quadrature oscillator. It's a circuit with 4 PWM outputs that are each 90° shifted. In Shabaz' blog, the oscillator is made with flip-flops, and cont...
    • 4 Aug 2021
  • Learning Xilinx Zynq: use RAM design for Altera Cyclone on Vivado and PYNQ

    Jan Cumps
    Jan Cumps
    Store 1024 12 bit values in a VHDL RAM design, and automatically test it.   This post uses the VHDL RAM design of Michael Kellett on a Zynq. You can store data and read it back. The design was done out of curiousity. To see how and when Block RA...
    • 2 Aug 2021
  • 6 Ways to Expand the Functionality of your Xilinx FPGA Board

    bhfletcher
    bhfletcher
    Every FPGA and Programmable Logic SoC development board has the ability to plug in add-on boards to expand the functionality of the basic board. When you are deciding on which board to use for your own learning or proof-of-concept, it's important to ...
    • 1 Aug 2021
  • Cheap Cyclone 10

    michaelkellett
    michaelkellett
    I've been following the discussions about the VIDOR4000 in the FPGA group. There was a giveaway associated with the Webinar but of course there will be sonme disapointed non-winners. If you want to get into playing with FPGAs one of the chea...
    • 31 Jul 2021
  • What Do You Think About Xilinx’s 16nm ZU1/2/3 InFO Package?

    jafoste4
    jafoste4
    Have you heard about Xilinx’s latest release in the 16nm line, the ZU1/2/3 InFO package? This package uses 60% less area and is roughly 70% thinner than standard Zynq UltraScale+ chip. InFO (for those that don’t know) stands for Integrated Fan-Out. T...
    • 30 Jul 2021
  • VIDOR 4000: Servo Interface

    jc2048
    jc2048
    Introduction Now a little project: a servo interface. This will give me a chance to experiment with some very simple communication between the microcontroller and the FPGA on my VIDOR 4000 board.  I'm going to have 8 servo channels...
    • 29 Jul 2021
  • VIDOR 4000: Clock Jitter

    jc2048
    jc2048
    Without connecting anything else to the VIDOR, the only clock we're given to work with is one that comes from the SAM microcontroller. Here it is on the VIDOR schematic, output from the SAM part and going into one of the dedicated clock inputs.&n...
    • 12 Jul 2021
  • VIDOR 4000: Johnson Counter

    jc2048
    jc2048
    Introduction In this blog Add Pynq-Z2 board to Vivado Jan refers to a Johnson counter. I struggled to remember what a Johnson counter actually was, but, for some reason, the number 4017 came to mind. Sure enough, the CD4017 CMOS logic device tur...
    • 10 Jul 2021
  • Learning Xilinx Zynq: FPGA based PWM generator with scroll wheel control

    Jan Cumps
    Jan Cumps
    DIY Test Instrumentation        Submit an EntrySubmit an Entry   Monthly Themes  | Monthly Poll  |  Back to homepage   This DIY instrument is a PWM generator with dead band support. It...
    • 9 Jul 2021
<>