Test & Tools
  • Technologies
  • More
Test & Tools
Documents Programmable Electronic Load
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 23 Dec 2016 1:09 PM Date Created
  • Last Updated Last Updated: 11 Oct 2020 8:05 AM
  • Views 23229 views
  • Likes 20 likes
  • Comments 401 comments
Related
Recommended

Programmable Electronic Load

Peter, Jon and Jan are building a programmable electronic load. This document is the common design sheet.

It's obviously work in progress. And fun.

 

image

 

 

We're building a programmable DC load. The focus is on making a real world working instrument.

Hardware and firmware are open source.

  • 20 V, 6 A
  • SCPI controlled

 

To keep this document readable, this main post gives an overview of the design.

All detailed explanations are broken out in separate posts.

 

Hardware

The load design is modular.

 

image

 

Two out of box modules:

  • MSP432 LaunchPad
  • LCD Shield (optional)

3 new designs

  • DAC-ADC module
  • Analog control module
  • Power module

 

DAC-ADC BoosterPack

image

This module is a generic, isolated DAC / ADC boosterpack. It's the interface between the analog controller and the microcontroller.

It can also be used outside this project, for your other analog - digital conversion needs.

The board design is broken out in a separate post: Programmable Electronic Load - DAC / ADC BoosterPack.

 

Analog Controller and Driver Board

This is the core of the analog constant current block. Here lives the circuit that will translate desired constant current into the driver signal for the power MOSFET.

It integrates the feedback coming from that power board. This is a closed analog control loop.

There are also components to provide the on-off functionality and buffers/amplifiers for the analog data-points that fly back to the ADC module.

image

The board, schematics and BOM are documented in Programmable Electronic Load - Analog Controller and Driver Board.

 

Power Module - the MOSFET Board with Fan

 

image

 

For details  of the design of the power stage, check Programmable Electronic Load - Power Stage.

 

BoosterPack Header Use and Pin Allocation

This info is broken out in a separate post: Programmable Electronic Load - BoosterPack Header Use.

 

Firmware

 

Prerequisites:

  • CCS 8 with MSP432 compiler TI v 16.12.0.STS or >
  • TI-RTOS for MSP43X, any SimpleLink version
  • MSP432 LaunchPad (not the black pre-prod because it's out of support)

 

The firmware is for the MSP432 microcontroller. But the harware can be driven from any controller, processor, PSoC or computer that can deliver i2c and power between 3V3 and 5V.

That includes Arduino, Raspberry Pi, BeagleBone, Warp7, IOT20xx, the ST Neo family, ... As long as they match that voltage range and have I2C master, it 'll work.

The ADC/DAC board takes care that the logic side is galvanicaly isolated from the power side (that is, if you leave the P1 and P2 jumpers open).

 

The only requirement is that you have a positive supply between 3V3 and 5V, a ground, and I2C signals (the board has I2C pull-ups that connect to the positive supply that you provide. If you don't want that (maybe your dev board already has 'm), leave R1 and R2 off.

ADC, DAC and Enable are all I2C driven.

 

GITHUB location: https://github.com/jancumps/msp432/tree/master/MSP432_SCPI_ElectronicLoad

download latest source files as a zip : https://github.com/jancumps/msp432/archive/master.zip

doxygen generated API documentation: https://jancumps.github.io/msp432

GIT artifacts don't contain CCS project files, only sources - get a zip with CCS project from the attachments at the end of this document.

image

 

SCPI interface and Error Handling

The SCPI commands are documented in this breakout post: SCPI interface.

 

UART Configuration

Together with SCPI, UART is the programming interface of this instrument.

The approach, and how to compile for USB or TTL, is documented in this breakout: UART.

 

RTOS and Posix Configuration

The TI-RTOS documentation is in breakout post RTOS Config.

 

LCD Display

Check here for a detailed explanation: LCD Display

The firmware supports SHARP LCD display,

 

 

 

image

image

 

ADC

 

I've broken out the ADC description to a separate post, because I'm working on improvements:

Programmable Electronic Load - ADC Firmware

 

 

DAC

 

DAC output is set on command, using RTOS MailBox and messaging.

The payload for a DAC message contains the DAC channel that needs to be set, and the value.

 

typedef struct MsgDAC {
    uint8_t module;
    uint16_t value;
} MsgDAC;

 

The DAC task is started by RTOS. It inialises the DAC settings, then waits until it receives a message.

 

void *threadDAC(void *arg0) {


    MsgDAC d_msg;
    d_daci2cTransaction.writeBuf = d_dactxBuffer;
    d_daci2cTransaction.readBuf = d_dacrxBuffer;
    d_daci2cTransaction.slaveAddress = DAC_I2C_ADDR;
    d_daci2cTransaction.writeCount = 3;
    d_daci2cTransaction.readCount = 0;


    mqd_t mq;
    struct mq_attr attr;


    attr.mq_flags = 0;
    attr.mq_maxmsg = 1;
    attr.mq_msgsize = MSGDAC_SIZE;
    attr.mq_curmsgs = 0;
    mq = mq_open(QUEUE_NAME_DAC, O_CREAT | O_RDONLY, 0644, &attr);


    while (1) {
        ssize_t bytes_read;
        bytes_read = mq_receive(mq, (char *)&d_msg, MSGDAC_SIZE, NULL);


        /* wait for mailbox to be posted by writer() */
        if (bytes_read) {
// ...

 

The waiting doesn't take processor time. RTOS takes care that it will only get a slice of clock cycles when there is a message.

Two things in the RTOS configuration make this happen:

The mailbox with room for exactly one message, and a receive event.


Because there is usually no message in the mailbox, the execution of the DAC logic becomes inactive at this line:

 

        bytes_read = mq_receive(mq, (char *)&d_msg, MSGDAC_SIZE, NULL);

 

When we send a DAC message somewhere else in the code (e.g.: when the user requests a new setting of the electronic load), RTOS reactivates the process and hands over the payload message.

The DAC task sets the output of the requested channel and returns to the point where it waits for a new message.

 

   while (1) {
        ssize_t bytes_read;
        bytes_read = mq_receive(mq, (char *)&d_msg, MSGDAC_SIZE, NULL);


        /* wait for mailbox to be posted by writer() */
        if (bytes_read) {
            d_dactxBuffer[0] = getAddressFromModule(d_msg.module); // set value direct
            d_dactxBuffer[1] = d_msg.value >> 8; // MSB
            d_dactxBuffer[2] = d_msg.value; // LSB
            if (! I2C_transfer(i2c_implGetHandle(), &d_daci2cTransaction)) {
//                System_printf("I2C Bus fault\n");
//                System_flush();
            }
        }
    }

 

You select the DAC channel by setting bit 2 and 1 in the control byte (tx_buffer[0]). There's a helper function that gives a correct control record.

 

// address 7 - 6: 0, load mode 5 - 4: 01 direct from i2c, 3: reserved 0, 2 - 1: channel select, 0: pwr down 0
#define DAC857X_CFG_H0 0b00010000
#define DAC857X_CFG_H1 0b00010010
#define DAC857X_CFG_H2 0b00010100
#define DAC857X_CFG_H3 0b00010110

 

 

static const uint8_t array_DAC857X_CFG_H[4] = {DAC857X_CFG_H0, DAC857X_CFG_H1, DAC857X_CFG_H2, DAC857X_CFG_H3};

/**
 * get the hex address for the requested DAC module
 */
uint8_t getAddressFromModule(uint8_t module) {
    return array_DAC857X_CFG_H[module];
}

 

Bits 7 - 3 and 0 are all fixed.

 

image

image

 

Input Enable

 

The functionality to activate and deactivate the load is documented here: Programmable Electronic Load - Input Enable Functionality .

 

Control Strategies

 

The firmware uses strategies to handle the different types of load operation (e.g. constant current, constant, voltage, ...).

 

A strategy is a set of functions that you can plug in, and that together run that particular operation type (this is a c version of the Gang of Four's Strategy Design Pattern).

The goal is to avoid that the firmware is riddled with if or switch statements whenever different behaviour is needed depending on the instrument's mode.

Each operation strategy will have the same set of functions that run the instrument in that mode.

The price to pay is not expensive - speed and memory burden is low. It is a little more complex to understand than the c++ version. Once you step trough it with a debugger, things become clear.

The code also tries to hide that we're using strategies

 

Currently starting to implement constant current strategy. The more difficult operation types can be added later, one by one, with not too much impact on the existing code across the firmware.

. Only the eload API (see below) knows about it. All code goes via that eload API.

API for the stategies is minimal now:

 

    controlFunction;
    getMode;
    getChar;

 

  

eload API

 

The eload API offers an abstraction layer for the strategies, so that the rest of the firmware doesn't have to know about it. It simplifies switching operation mode and driving the instrument.

 

Example: The eload API offers a simple function eloadGetMode() to check what the instrument's current mode is.

 

eload_mode eloadGetMode() {

    return getControlStrategy()->getMode();

}

 

In the background, it uses the strategy mechanism to fetch the mode from the currently active strategy and call the implementation function.

 

return getControlStrategy()->getMode();

 

The eload API also has the common eload functions that don't need a strategy because they are always valid, regardless of mode.

 

Calibration and Configuration Data

 

The functionality to store calibration and configuration data in Flash is described in a separate article: Programmable Electronic Load - Calibration Data in Flash.

The calibration and configuration procedures are documented in Programmable Electronic Load - Calibration Steps

 

Changes To Standard MSP_EXP432P401R.c

 

The standard file generated by the TI-RTOS application wizard has defaults for peripherals.

The following has changed: none - I removed this section because with the external ADC/DAC board and the SimpleLink RTOS version, everything is kept standard.

 

Remote Software

 

Teminal

 

Serial communication to the USB UART port.

9600/8/1/None

image

SCPI is a non-echoing protocol. To make the characters you type show in the Terminal, set Local echo to Force on.

If you also set Local line editing to Force on, you have the opportunity to correct characters in the current line before they are sent to the serial port.

image

 

Test:

*IDN?;SYST:ERR:COUN?

Should return

THEBREADBOARD,ELECTRONICLOAD,0,01.00;0

 

Windows GUI

 

There are two image. A .NET made by Peter, a Java version made by Jan.

 

The .net GUI supports reading the 4 ADCs, setting one of the DACs abd shoot any SCPI command.

There's a window for SCPI output and a status window that shows SCPI errors.

image

Source and binary available from https://github.com/thebreadboard/SCPI_DC_LOAD_WIN

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

The Java GUI is made as a POC that cross-platform instrument GUIs are possible.

It allows for switching the load on and off, set constant current and replicate the LCD values.

Additionally, you can requesst error status and run arbitrary SCPI commands.

Programmable Electronic Load - Java GUI Part 1: Basic Functionality

 

image

 

 

LabVIEW

 

The instrument comes with a LabVIEW library: Programmable Electronic Load - Write a LabVIEW Library part 1: Initialise Block

image

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

 

Related blog

Programmable Electronic Load - Input Enable Functionality
Programmable Electronic Load - Power Stage
Programmable Electronic Load - Temperature Protection
Programmable Electronic Load - DAC / ADC BoosterPack
Programmable Electronic Load - Analog Controller and Driver Board
Programmable Electronic Load - SCPI interface and Error Handling
Programmable Electronic Load - UART
Programmable Electronic Load - RTOS Config
Programmable Electronic Load - Calibration Data in Flash
Programmable Electronic Load - Calibration Steps
Programmable Electronic Load - LCD Display
Programmable Electronic Load - ADC Firmware
Programmable Electronic Load - Current Sense Circuit
Programmable Electronic Load - BoosterPack Header Use
Programmable Electronic Load - ToDo and Done
Robert Peter Oakes articles:
Electronic DC Load - Design and Build to test PSU Project
youtube: Electronic DC Load Design and Testing
youtube: Full Build Analogue DC Load
youtube: Electronic DC Load - Performance Improvements
Raspberry PI 2, Fun with I2C DACs and ADC's
jc2048 articles:
Programmable Electronic Load: Dynamic Behaviour: Part 1 Overview
Programmable Electronic Load: Dynamic Behaviour: Part 2 The Servo Loop
Programmable Electronic Load: Dynamic Behaviour: Part 3 Effect of Output Inductance
Programmable Electronic Load: Dynamic Behaviour: Part 4 Effect of Output Voltage Change
Programmable Electronic Load: Dynamic Behaviour: Part 5 Stability
Programmable Load Build
Jan Cumps articles:
Programmable Electronic Load - ADC and DAC BoosterPack test
Programmable Electronic Load - Analyse the Summing Node Zero Point
Programmable Electronic Load - Measurements Part 1: Control Circuit
Java GUI
Programmable Electronic Load - Java GUI Part 1: Basic Functionality
Programmable Electronic Load - Java GUI Part 2: Support for Current Mode, Input On/Off, Error Log
LabView
Programmable Electronic Load - Write a LabVIEW Library part 1: Initialise Block
Programmable Electronic Load - Write a LabVIEW Library part 2: Read Output Block
Programmable Electronic Load - Write a LabVIEW Library part 3: Close Block
Programmable Electronic Load - Write a LabVIEW Library part 4: Function Set Block
Programmable Electronic Load - Write a LabVIEW Library part 5: Input Control Block
Programmable Electronic Load - Write a LabVIEW Library part 6: Raw DAC Block
Programmable Electronic Load - Write a LabVIEW Library part 7: Raw ADC Block
Programmable Electronic Load - Automating a DC Switcher Efficiency Test with LabVIEW
Programmable Electronic Load - LabVIEW Test Automation: Characterise the Instrument
Programmable Electronic Load - LabVIEW Test Automation: Characterise the Instrument Pt 2: Oscilloscope Measurements
Example LabVIEW Scenario: test a design with a Rigol PSU and a Keithley DMM
TI-RTOS: Switching to the SimpleLink Distribution
Switch from TI-RTOS to SimpleLink POSIX: Threads and Semaphores
Switch from TI-RTOS to SimpleLink POSIX: EEPROM API
Switch from TI-RTOS to SimpleLink POSIX: From MailBox to Message Queue
Switch from TI-RTOS to SimpleLink POSIX: LCD Display Driver
Switch from TI-RTOS to SimpleLink POSIX: Sleep when Idle
Attachments:
pcb_proto.zip
eload_v1_20170227.zip
eload_1_2a.zip
https://community.element14.com/cfs-file/__key/communityserver-wikis-components-files/00-00-00-00-21/bom.ods
MSP432_SCPI_ElectronicLoad_20180102.zip
eload_power_20180104.zip
eload.zip
eload_examples.zip
MSP432_SCPI_ElectronicLoad_20180514.zip
measureefficiency.zip
measureefficiency_5V_10V_600mA_RAW.zip
MSP432_SCPI_ElectronicLoad_v_00_0_0_1_20180914.zip
MSP432_SCPI_ElectronicLoad_20190706.zip
  • load_cell
  • metrology
  • msp432
  • ti-rtos
  • launchpad
  • laboratory
  • instrument
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 6 years ago +4
    Revisiting the eLoad design - there's definitely room for approval. The very low currency (minus 3 mA) is awful. And the calibration is off. I've set it to 0.5 A- and it thinks it's drawing that current…
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to Jan Cumps +3
    All components are now in and soldered. Time to test. I'll first check out the power rails in isolation. If they are ok. I'll mount LaunchPad, LCD and and DAC board and do measurements. Hang on
  • Jan Cumps
    Jan Cumps over 8 years ago +3
    good news: I finally got persistent saving of calibration/setup sorted out. At first I had issues getting the in-ROM Flash api recognised by the compiler when using it with RTOS. That turned out to be…
Parents
  • jc2048
    jc2048 over 9 years ago

    I'm back again, after a bit of shameless bribery from Jan (I get one of his spare ADC/DAC booster boards in return for some more thoughts and comments).

     

    I'm interested in how the control loop works: why there's such a large offset at the bottom end of the current range (and what can be done about it) and what the advantages are (if any) of the summing arrangement (which I'm not familiar with at all).

     

    I don't have much of a background in analogue design, so I'm learning this as I go along. (Please shout if you see me getting things wrong.)

     

    Input Bias

     

    Here's the control loop in a simplified form so that it's easier to see the control action. (I've stripped away all the frequency dependent stuff, so we're looking at dc here - keep in mind that there will be other complications at ac.)

     

     

    image

     

    Here's how I see the control operating. The control input is a positive voltage in proportion to the desired current. The signal fed back by the current sense amplifier is a negative voltage (it's negative because the gain is -7.8, not 7.8). The op amp acts to try and make both of its inputs the same voltage, so with the two resistors the same value, the fed back voltage will match the control voltage, except for its sign. If the control were set to 1.95V, the opamp would control the MOSFET to give 5A through the sense resistor so that the fed back voltage were -1.95V and the voltage at the + input to the opamp was then 0V.

     

    Now, what is the current through the pair of resistors for different input voltages? Let's pretend for a moment that the opamp is perfect and doesn't load the midpoint at all.

     

    Input voltage    % of full scale    Desired Current    Resistor Current
    1.95                 100                      5A                       19.5uA
    195mV             10                       500mA                1.95uA
    19.5mV             1                       50mA                   195nA
    1.95mV             0.1                    5mA                     19.5nA

     

    That seems fine (perhaps 'fine' isn't the word - it seems to me to be a fundamental flaw of the arrangement the way the control current falls off for low control voltages - maybe a doubtful 'plausible' or 'possible' might be better) until we look at the datasheet for the opamp and see this

     

    image

     

     

     

    In case it's not clear why the current is negative (flowing out of the chip), here's the equivalent schematic from the datasheet where we can see that the input transistors are PNP

     

     

    image

     

    The Input Bias Current that flows out of the bases of the transistors is typically -0.7uA [for supplies of +-15V]. If we compare that to the current through the two resistors, we can immediately see that there is going to be a problem at the lower end of the input control voltage range where the bias current is much higher than the current through the resistors.

     

    Can the circuit be improved? My first thoughts on that would include the following.

     

    One option would be to decrease the size of the resistors. If we made them 10k, rather than 100k, the resistor currents would be ten times higher. That would help a bit. How far could we go with that? It looks like the current sense amplifier can drive 1k or 2k sensibly. I don't know about the DAC.

     

    Another thing we could do is to be very rigorous about balancing the inputs to the opamps. Whilst the bias current is fairly high, both inputs will match well [the transistors will be almost identical being fabbed on the same piece of silicon] and the currents tend to cancel if we can make the resistance looking out of the terminal the same for both the input pins. A problem there, though, is the frequency selective network feeding back locally around the opamp - what frequency do we make the inputs balance for? It has to be DC, but then it's going to change as the frequency goes up.

     

    A more obvious option would be to substitute an op-amp with a lower input bias current. There are bipolar op-amps with much lower bias currents (they include extra circuitry to offset the current internally), MOSFET-input op-amps have an input bias current in the pA area [mostly the protection diode leakage], and FET inputs are almost as good. However it's complicated by temperature [leakage currents climb quickly with increased temperature], so substituting an op-amp is a bit more complicated than just choosing on the basis of one parameter (and we may just be swapping one problem for another).

     

    There's also the question of whether it's good to stick with the summing junction approach.

     

    Before considering that any further, I'm going to see if I can look at the stability and the frequency response of the current circuit - partly to find out how to do it, partly to understand what bearing the summing arrangement has on the stability, and also because I want to see what effect output loads have and what a reasonable spec might be for such an instrument.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jc2048
    jc2048 over 9 years ago

    I'm back again, after a bit of shameless bribery from Jan (I get one of his spare ADC/DAC booster boards in return for some more thoughts and comments).

     

    I'm interested in how the control loop works: why there's such a large offset at the bottom end of the current range (and what can be done about it) and what the advantages are (if any) of the summing arrangement (which I'm not familiar with at all).

     

    I don't have much of a background in analogue design, so I'm learning this as I go along. (Please shout if you see me getting things wrong.)

     

    Input Bias

     

    Here's the control loop in a simplified form so that it's easier to see the control action. (I've stripped away all the frequency dependent stuff, so we're looking at dc here - keep in mind that there will be other complications at ac.)

     

     

    image

     

    Here's how I see the control operating. The control input is a positive voltage in proportion to the desired current. The signal fed back by the current sense amplifier is a negative voltage (it's negative because the gain is -7.8, not 7.8). The op amp acts to try and make both of its inputs the same voltage, so with the two resistors the same value, the fed back voltage will match the control voltage, except for its sign. If the control were set to 1.95V, the opamp would control the MOSFET to give 5A through the sense resistor so that the fed back voltage were -1.95V and the voltage at the + input to the opamp was then 0V.

     

    Now, what is the current through the pair of resistors for different input voltages? Let's pretend for a moment that the opamp is perfect and doesn't load the midpoint at all.

     

    Input voltage    % of full scale    Desired Current    Resistor Current
    1.95                 100                      5A                       19.5uA
    195mV             10                       500mA                1.95uA
    19.5mV             1                       50mA                   195nA
    1.95mV             0.1                    5mA                     19.5nA

     

    That seems fine (perhaps 'fine' isn't the word - it seems to me to be a fundamental flaw of the arrangement the way the control current falls off for low control voltages - maybe a doubtful 'plausible' or 'possible' might be better) until we look at the datasheet for the opamp and see this

     

    image

     

     

     

    In case it's not clear why the current is negative (flowing out of the chip), here's the equivalent schematic from the datasheet where we can see that the input transistors are PNP

     

     

    image

     

    The Input Bias Current that flows out of the bases of the transistors is typically -0.7uA [for supplies of +-15V]. If we compare that to the current through the two resistors, we can immediately see that there is going to be a problem at the lower end of the input control voltage range where the bias current is much higher than the current through the resistors.

     

    Can the circuit be improved? My first thoughts on that would include the following.

     

    One option would be to decrease the size of the resistors. If we made them 10k, rather than 100k, the resistor currents would be ten times higher. That would help a bit. How far could we go with that? It looks like the current sense amplifier can drive 1k or 2k sensibly. I don't know about the DAC.

     

    Another thing we could do is to be very rigorous about balancing the inputs to the opamps. Whilst the bias current is fairly high, both inputs will match well [the transistors will be almost identical being fabbed on the same piece of silicon] and the currents tend to cancel if we can make the resistance looking out of the terminal the same for both the input pins. A problem there, though, is the frequency selective network feeding back locally around the opamp - what frequency do we make the inputs balance for? It has to be DC, but then it's going to change as the frequency goes up.

     

    A more obvious option would be to substitute an op-amp with a lower input bias current. There are bipolar op-amps with much lower bias currents (they include extra circuitry to offset the current internally), MOSFET-input op-amps have an input bias current in the pA area [mostly the protection diode leakage], and FET inputs are almost as good. However it's complicated by temperature [leakage currents climb quickly with increased temperature], so substituting an op-amp is a bit more complicated than just choosing on the basis of one parameter (and we may just be swapping one problem for another).

     

    There's also the question of whether it's good to stick with the summing junction approach.

     

    Before considering that any further, I'm going to see if I can look at the stability and the frequency response of the current circuit - partly to find out how to do it, partly to understand what bearing the summing arrangement has on the stability, and also because I want to see what effect output loads have and what a reasonable spec might be for such an instrument.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago in reply to jc2048

    Forgot to also mention - re the summing junction. This is exactly the same as connecting the feedback 100K to the output of the op-amp (Making it a stand alone gain without the rest of the loop) and is how an inverting configured op-amp works, we have simply extended the feedback to include the sense resistor and the mosfet.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago in reply to jc2048

    Nice work there Jon

     

    A Lot of the solution I think would be in selecting the right Op-Amp, one with hi impedance inputs for instance.

    One of the reasons for selecting such high value resistors was to significantly reduce the chance of frying the electronics if something went wrong with the power stage, I have already fried the entire project with my old design because the common mode volts went way out of range (Up to the source voltage of 30V), the resultant current I think exceeded the input diode protection (10mA) and the rest was history image. So 100K with even 60-100V source to the load leads to a max of only 1mA flowing into the protection diodes, well within its safe current.

     

    So could we reduce the values. Yes of course but I would be tempted to stay well away from the 10mA max current in a failure mode (Or a simple spike getting through), so perhaps not less than about 20K = 5mA in fault condition.

     

    Hope this helps to understand my choices.

     

    Oh, the summing junction is just a very simple way of balancing setpoint with measured and if you make both resistors the same with the same characteristics then there always going to be the same sum even if they get hot etc. They should drift the same image. Also if it's good enough for Agilent, its good enough for me image and it keeps the component count small, especially for the silicon.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to jc2048

    correction: 2 adc/dac pcbs image