When I need to run the generator on Bonesnapper Ridge, it usually means that it's raining or snowing and generally muddy. The walk from the house to the generator in those conditions is doable, but not my favorite. There could be many solutions to this, but for me, it's building something that works exactly the way I want it! In this episode, I build a remote generator start for a Honda EU-7000is that is controlled via WiFi and a custom made panel with displays.
Watch the Video:
Downloads and Links:
- Download Code and CAD Files: https://github.com/KalebTheMaker/GeneratorRemote
Bill of Material:
Product Name | Manufacturer | Quantity | Buy Kit |
---|---|---|---|
Arduino NANO IOT33 Wifi | ABX00032 | 2 | Buy Now |
LED 7-SEG DISPLAY, COM CATHOD, GRN | TDCG1060M | 6 | Buy Now |
MAX7221ENG+ Display Dirver 8 digit | MAX7221ENG+ | 4 | Buy Now |
Rocker Switch | SRJ22A3BBBNN | 2 | Buy Now |
SWITCH, SPST-NO, 0.4A, 32VAC, ROUND, RED | 59-112 | 4 | Buy Now |