Raspberry Pi Auto Etch A Sketch
element14 presents | daftmike's VCP Profile | Project Videos
In this video Mike builds an automatic Etch A Sketch machine using stepper motors and 3D printed gears. |
Bill of Material:
Product Name | Manufacturer | Quantity | Buy KitBuy Kit |
---|---|---|---|
Raspberry Pi 3 Model B+, BCM2837B0 SoC, IoT, PoE, NOOBS Included | RASPBERRY-PI | 1 | Buy NowBuy Now |
Raspberry Pi DC Stepper Motor Hat Develo | ADAFRUIT | 1 | Buy NowBuy Now |
3D Printer Filament, 1.75 mm, PLA, Red, 1 kg | MULTICOMP | 1 | Buy NowBuy Now |
Stepper Motor, High Torque, DC, 0.5 N-m, 1.8 A, Two Phase, 1.75 ohm, 3.3 mH | NANOTEC | 1 | Buy NowBuy Now |
CONTINUOUS ROTATION SERVO | ADAFRUIT | 1 | Buy NowBuy Now |
Arduino Flip Code:
/* ================================================================================ GY-521 IMU test code for flipping the etch a sketch - daftmike 2018 ================================================================================ */ #include <Wire.h> #include <Servo.h> // Servo is attached to pin 5 Servo servo; const int servoPin = 5; // Variables used for the IMU readings long accelX, accelY, accelZ; float gForceX, gForceY, gForceZ; long gyroXCali = 0, gyroYCali = 0, gyroZCali = 0; long gyroXPresent = 0, gyroYPresent = 0, gyroZPresent = 0; long gyroXPast = 0, gyroYPast = 0, gyroZPast = 0; float rotX, rotY, rotZ; float angleX = 0, angleY = 0, angleZ = 0; long timePast = 0; long timePresent = 0; // Variables used to keep track of the 'flip' bool flipStarted = 0; bool flipFinished = 0; int flips = 0; int servoDir = 90; // String to hold the serial data from the Pi String piMsg; // Speed, angle and number of 'flips' const int forwardSpeed = 60; const int backwardSpeed = 180; const int numFlips = 5; const int lowAngle = -140; const int midAngle = -120; /*================================================================================*/ void setup() { Serial.begin(9600); // start the serial port Wire.begin(); // start i2c setUpMPU(); // start IMU coms calibrateGyroValues(); timePresent = millis(); // time reference for IMU readings } /*================================================================================*/ void loop() { readAndProcessAccelData(); readAndProcessGyroData(); readPi(); } /*================================================================================*/ void servoFlip() { if (servoDir == 90) { servo.attach(servoPin); servoDir = forwardSpeed; servo.write(servoDir); Serial.println("flip started, servo moving forward..."); flipStarted = 1; } if (flipStarted == 1) { if (servoDir == forwardSpeed && angleX < lowAngle && flips < numFlips) { servoDir = backwardSpeed; servo.write(servoDir); Serial.println("servo backward..."); flips++; Serial.print("flip number: "); Serial.println(flips); } if (servoDir == backwardSpeed && angleX > midAngle && flips < numFlips) { servoDir = forwardSpeed; servo.write(servoDir); Serial.println("servo forward..."); flips++; Serial.print("flip number: "); Serial.println(flips); } if (servoDir == backwardSpeed && -2 < angleX) { Serial.println("turning servo OFF..."); servo.detach(); servoDir = 90; flips = 0; flipStarted = 0; delay(2000); setUpMPU(); calibrateGyroValues(); } } } void readPi() { // read data from the serial port into a string to check for messages if (Serial.available()) { piMsg = Serial.readString(); if (piMsg == "flip") { servoFlip(); } else if (piMsg == "cali") { Serial.println("calibrating gyro values..."); setUpMPU(); calibrateGyroValues(); } } } void setUpMPU() { // power management Wire.beginTransmission(0b1101000); // Start the communication by using address of MPU Wire.write(0x6B); // Access the power management register Wire.write(0b00000000); // Set sleep = 0 Wire.endTransmission(); // End the communication // configure gyro Wire.beginTransmission(0b1101000); Wire.write(0x1B); // Access the gyro configuration register Wire.write(0b00000000); Wire.endTransmission(); // configure accelerometer Wire.beginTransmission(0b1101000); Wire.write(0x1C); // Access the accelerometer configuration register Wire.write(0b00000000); Wire.endTransmission(); } void calibrateGyroValues() { for (int i = 0; i < 5000; i++) { getGyroValues(); gyroXCali = gyroXCali + gyroXPresent; gyroYCali = gyroYCali + gyroYPresent; gyroZCali = gyroZCali + gyroZPresent; } gyroXCali = gyroXCali / 5000; gyroYCali = gyroYCali / 5000; gyroZCali = gyroZCali / 5000; } void readAndProcessAccelData() { Wire.beginTransmission(0b1101000); Wire.write(0x3B); Wire.endTransmission(); Wire.requestFrom(0b1101000, 6); while (Wire.available() < 6); accelX = Wire.read() << 8 | Wire.read(); accelY = Wire.read() << 8 | Wire.read(); accelZ = Wire.read() << 8 | Wire.read(); processAccelData(); } void processAccelData() { gForceX = accelX / 16384.0; gForceY = accelY / 16384.0; gForceZ = accelZ / 16384.0; } void readAndProcessGyroData() { gyroXPast = gyroXPresent; // Assign Present gyro reaging to past gyro reading gyroYPast = gyroYPresent; // Assign Present gyro reaging to past gyro reading gyroZPast = gyroZPresent; // Assign Present gyro reaging to past gyro reading timePast = timePresent; // Assign Present time to past time timePresent = millis(); // get the current time in milli seconds, it is the present time getGyroValues(); // get gyro readings getAngularVelocity(); // get angular velocity calculateAngle(); // calculate the angle } void getGyroValues() { Wire.beginTransmission(0b1101000); // Start the communication by using address of MPU Wire.write(0x43); // Access the starting register of gyro readings Wire.endTransmission(); Wire.requestFrom(0b1101000, 6); // Request for 6 bytes from gyro registers (43 - 48) while (Wire.available() < 6); // Wait untill all 6 bytes are available gyroXPresent = Wire.read() << 8 | Wire.read(); // Store first two bytes into gyroXPresent gyroYPresent = Wire.read() << 8 | Wire.read(); // Store next two bytes into gyroYPresent gyroZPresent = Wire.read() << 8 | Wire.read(); // Store last two bytes into gyroZPresent } void getAngularVelocity() { rotX = gyroXPresent / 131.0; rotY = gyroYPresent / 131.0; rotZ = gyroZPresent / 131.0; } void calculateAngle() { // same equation can be written as // angleZ = angleZ + ((timePresentZ - timePastZ)*(gyroZPresent + gyroZPast - 2*gyroZCalli)) / (2*1000*131); // 1/(1000*2*131) = 0.00000382 // 1000 --> convert milli seconds into seconds // 2 --> comes when calculation area of trapezium // substacted the callibated result two times because there are two gyro readings angleX = angleX + ((timePresent - timePast) * (gyroXPresent + gyroXPast - 2 * gyroXCali)) * 0.00000382; angleY = angleY + ((timePresent - timePast) * (gyroYPresent + gyroYPast - 2 * gyroYCali)) * 0.00000382; angleZ = angleZ + ((timePresent - timePast) * (gyroZPresent + gyroZPast - 2 * gyroZCali)) * 0.00000382; } void printData() { Serial.print("X : "); Serial.print(angleX); Serial.print("° | Y : "); Serial.print(angleY); Serial.print("° | Z : "); Serial.print(angleZ); Serial.println("°"); }
Supporting Files:
for access to all the supporting files you will need to replicate this build!